2021-06-14 9:02 AM
Thats a question that has bothered me for a while. When receiving FDCAN messages, I can specify a watermark on how many bytes the interrupt triggers.
How exactly does it work?
If I have a message of 8 bytes and I set the watermark to 1 byte, does the interrupt trigger 8 times?
And then do I always have 1Byte in the payload? Or the entire message.
Besides, what's the best way to check? Because currently, every time I debug and go to the message in the interrupt to see what is in RxData, I already see my complete message.
I actually want (especially with lower bit rates) that if the first part of a CAN message is already available, i can analyze its in order to send it out if necessary.
Heres Config FDCAN ->
void MX_FDCAN1_Init(void)
{
/*
Bit time parameter | Nominal
---------------------------|--------------
fdcan_ker_ck | 20 MHz
Time_quantum (tq) | 50 ns
Synchronization_segment | 1 tq
Propagation_segment | 3 tq
Phase_segment_1 | 8 tq
Phase_segment_2 | 8 tq
Synchronization_Jump_width | 8 tq
Bit_length | 20 tq = 1 µs
Bit_rate | 1.0 MBit/s
*/
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = ENABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = ENABLE;
/* Nominal Time Quanta */
hfdcan1.Init.NominalPrescaler = round(1e6/CANBaudRate);
hfdcan1.Init.NominalSyncJumpWidth = 8;
hfdcan1.Init.NominalTimeSeg1 = 11;
hfdcan1.Init.NominalTimeSeg2 = 8;
/* Derzeit fest eingestellt für 2MBit/s */
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 4;
hfdcan1.Init.DataTimeSeg1 = 5;
hfdcan1.Init.DataTimeSeg2 = 4;
hfdcan1.Init.MessageRAMOffset = 0;
hfdcan1.Init.StdFiltersNbr = 1;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.RxFifo0ElmtsNbr = 2;
hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.RxFifo1ElmtsNbr = 0;
hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.RxBuffersNbr = 0;
hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
hfdcan1.Init.TxEventsNbr = 0;
hfdcan1.Init.TxBuffersNbr = 0;
hfdcan1.Init.TxFifoQueueElmtsNbr = 2;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN FDCAN1_Init 2 */
HAL_StatusTypeDef Error;
FDCAN_FilterTypeDef sFilterConfig;
/* Configure Rx filter */
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterType = FDCAN_FILTER_MASK;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x111;
sFilterConfig.FilterID2 = 0x000; /* For acceptance, MessageID and FilterID1 must not match */
Error = HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig);
if(Error != HAL_OK) Error_Handler();
/* Configure global filter to reject all non-matching frames */
Error = HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_REJECT_REMOTE, FDCAN_REJECT_REMOTE);
if(Error != HAL_OK) Error_Handler();
/* Configure Rx FIFO 0 watermark to 1 */
Error = HAL_FDCAN_ConfigFifoWatermark(&hfdcan1, FDCAN_CFG_RX_FIFO0, 1);
if(Error != HAL_OK) Error_Handler();
/* Activate Rx FIFO 0 watermark notification */
Error = HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_WATERMARK, 0);
if(Error != HAL_OK) Error_Handler();
/* Start the FDCAN module */
Error = HAL_FDCAN_Start(&hfdcan1);
if(Error != HAL_OK) Error_Handler();
}And of course the Interupt where the CAN Message is read ->
void FDCAN1_IT0_IRQHandler(void)
{
FDCAN_RxHeaderTypeDef RxHeader;
uint8_t RxData[8];
HAL_FDCAN_IRQHandler(&hfdcan1);
HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
HAL_FDCAN_GetRxMessage(&hfdcan1, FDCAN_RX_FIFO0, &RxHeader, RxData);
if((RxHeader->DataLength >> 16) == FDCAN_DLC_BYTES_0) return;
can_interpret(&RxHeader, RxData);
}I am incredibly sorry if I am wrong with such questions here in the forum..
But thanks for everyone who takes the time to help me! :D
2021-06-15 1:58 AM
Or have I completely misunderstood something and the interrupt only triggers when the CAN message has been fully received?
And the watermark only describes the size of the total number of databytes received?