Skip to main content
JA1
Associate
August 4, 2021
Question

How do I guarantee that st-flash --reset write will reliably reset STM32G070 after write completion?

  • August 4, 2021
  • 3 replies
  • 2321 views

When flashing a bin file to a blank/erased STM32G070 the --reset option does not consistently reset the processor after flash.

The first couple times I did this it worked. Now it is not.

A snippet of the output from a failed example using the command 'st-flash --reset --debug write foo.bin 0x08000000' is below:

2021-08-04T16:40:02 DEBUG usb.c: r_idx (16) = 0x81000000
2021-08-04T16:40:02 DEBUG common.c: *** stlink_jtag_reset ***
2021-08-04T16:40:02 DEBUG common.c: *** stlink_reset ***
2021-08-04T16:40:02 WARN usb.c: NRST is not connected
2021-08-04T16:40:02 DEBUG usb.c: Using reset through SYSRESETREQ
2021-08-04T16:40:02 DEBUG common.c: *** stlink_soft_reset ***
2021-08-04T16:40:02 DEBUG common.c: *** stlink_write_debug32 0xa05f0003 to 0xe000edf0
2021-08-04T16:40:02 DEBUG common.c: *** stlink_write_debug32 0x01000500 to 0xe000edfc
2021-08-04T16:40:02 DEBUG common.c: *** stlink_read_debug32 0x01030003 at 0xe000edf0
2021-08-04T16:40:02 DEBUG common.c: *** stlink_write_debug32 0x05fa0004 to 0xe000ed0c
2021-08-04T16:40:02 DEBUG common.c: *** stlink_read_debug32 0x03000001 at 0xe000edf0
2021-08-04T16:40:02 DEBUG common.c: *** stlink_read_debug32 0x01000001 at 0xe000edf0
2021-08-04T16:40:02 DEBUG common.c: *** stlink_write_debug32 0x0000001f to 0xe000ed30
2021-08-04T16:40:02 DEBUG common.c: *** stlink_exit_debug_mode ***
2021-08-04T16:40:02 DEBUG common.c: *** stlink_write_debug32 0xa05f0000 to 0xe000edf0
2021-08-04T16:40:02 DEBUG common.c: *** stlink_close ***

Setup:

  • OS: Ubuntu 18.04
  • st-flash version: v1.6.1-224-g9956bde-dirty
This topic has been closed for replies.

3 replies

TDK
August 5, 2021

Perhaps use STM32CubeProgrammer CLI instead, or report the issue to the people who make st-flash.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
August 5, 2021

Newer STM32 need to be power cycled if programmed from blank, it maps boot from ROM if it detects it is empty and that gets latched in a way that a reset doesn't clear.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JA1
JA1Author
Associate
August 6, 2021

Is this documented anywhwere? I've searched for this, but couldn't find it.