2015-01-18 12:19 PM
hi
How do I assign a TUS variable cont TUS = cont; How do I ? thanks #include <stm32f10x.h> #include <stm32f10x_conf.h> #include <stm32f10x_rcc.h> #include <stm32f10x_gpio.h> #define PORT GPIOB #define TUS GPIO_Pin_1 char cont; int main(void) { RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); GPIO_StructInit(&GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 ; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(PORT, &GPIO_InitStructure); // TUS = cont; // }2015-01-18 01:07 PM
Awkwardly posed...
Writing GPIO_SetBits(GPIOB, GPIO_Pin_1); GPIO_ResetBits(GPIOB, GPIO_Pin_1); GPIO_WriteBit(GPIOB, GPIO_Pin_1, state); GPIOB->ODR = (GPIOB->ODR & ~GPIO_Pin_1) | (state ? GPIO_Pin_1 : 0); Reading state = GPIO_ReadInputDataBit(GPIOC, GPIO_Pin_3); state = GPIOC->IDR & GPIO_Pin_3;2015-01-18 01:19 PM
Thank you