cancel
Showing results for 
Search instead for 
Did you mean: 

How ''Disable Read Out Protection'' ?

musatoff
Associate II
Posted on October 03, 2012 at 18:13

I have demoboard with STM32F417 and ST-Link v2. After some software fault, read out protection was activated. STlink utility print 

20:07:57 : Connected via SWD.

20:07:57 : Device ID:0x411 

20:07:57 : Device family :STM32F4xx

20:07:57 : Cannot read memory!

                  Disable Read Out Protection and retry.

What I mast to do to disable read out protection. I can't to do full erase of chip with the same error:

ST-LINK_CLI.exe -c SWD UR -OB RDP=0 WRP=0xFFFFFFFF -ME

STM32 ST-LINK CLI v1.3.0

STM32 ST-LINK Command Line Interface

Connected via SWD.

Device ID:0x411 

Device family :STM32F4xx

Updating option bytes...

Could not update the option bytes!

Full chip erase...

Read out protection is activated

10 REPLIES 10
Dhananjay Khairnar
Associate II
Posted on April 27, 2017 at 08:59

Take any other HEX file and programe it. It will remove read out protection