2012-10-03 09:13 AM
I have demoboard with STM32F417 and ST-Link v2. After some software fault, read out protection was activated. STlink utility print
20:07:57 : Connected via SWD.
20:07:57 : Device ID:0x411 20:07:57 : Device family :STM32F4xx20:07:57 : Cannot read memory! Disable Read Out Protection and retry.What I mast to do to disable read out protection. I can't to do full erase of chip with the same error:ST-LINK_CLI.exe -c SWD UR -OB RDP=0 WRP=0xFFFFFFFF -ME
STM32 ST-LINK CLI v1.3.0STM32 ST-LINK Command Line InterfaceConnected via SWD.Device ID:0x411 Device family :STM32F4xxUpdating option bytes...Could not update the option bytes!Full chip erase...Read out protection is activated2017-04-26 11:59 PM
Take any other HEX file and programe it. It will remove read out protection