How Disable global interrupt with ARM 32F0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-02 12:15 AM
Dear All
Following syntax does nit disable the global interruptPlease advice uint32_t PriMask = 0x01; //void __enable_irq (void);//Global Interrupt enable (using the instruction CPSIE i) void __set_PRIMASK (uint32_t PriMask );// M0, M3PRIMASK = value// Assign value to Priority Mask Register (usingthe instruction MSR) //void __disable_irq(void); //void __diasable_irq(void); //void __set_PRIMASK (uint32_t __set_PRIMASK); //uint32_t __get_PRIMASK(void)It is seem to be ''PRIMASK;bit does not disableplease advice how disable PRIMASK BIT disable with CMSIS source codeThanks in advance- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-02 1:43 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-02 5:22 AM
Why?
__get_PRIMASK(), and __set_PRIMASK() should allow you to check/set/clear bit 0Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-03 8:49 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-03 9:15 AM
Bit 5 of ICER one might presume from the documentation
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-04 7:50 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-04 8:14 AM
There's a one-to-one relationship with the IRQ#
STM32F0308-Discovery_FW_V1.0.1\Libraries\CMSIS\Device\ST\STM32F0xx\Include\stm32f0xx.h#if defined (STM32F0XX_MD) || defined (STM32F030X8)
/****** STM32F0XX_MD and STM32F030X8 specific Interrupt Numbers *************************************/
WWDG_IRQn = 0, /*!< Window WatchDog Interrupt */
PVD_IRQn = 1, /*!< PVD through EXTI Line detect Interrupt */
RTC_IRQn = 2, /*!< RTC through EXTI Line Interrupt */
FLASH_IRQn = 3, /*!< FLASH Interrupt */
RCC_IRQn = 4, /*!< RCC Interrupt */
EXTI0_1_IRQn = 5, /*!< EXTI Line 0 and 1 Interrupts */
EXTI2_3_IRQn = 6, /*!< EXTI Line 2 and 3 Interrupts */
EXTI4_15_IRQn = 7, /*!< EXTI Line 4 to 15 Interrupts */
TS_IRQn = 8, /*!< TS Interrupt */
DMA1_Channel1_IRQn = 9, /*!< DMA1 Channel 1 Interrupt */
DMA1_Channel2_3_IRQn = 10, /*!< DMA1 Channel 2 and Channel 3 Interrupts */
DMA1_Channel4_5_IRQn = 11, /*!< DMA1 Channel 4 and Channel 5 Interrupts */
ADC1_COMP_IRQn = 12, /*!< ADC1, COMP1 and COMP2 Interrupts */
TIM1_BRK_UP_TRG_COM_IRQn = 13, /*!< TIM1 Break, Update, Trigger and Commutation Interrupts */
TIM1_CC_IRQn = 14, /*!< TIM1 Capture Compare Interrupt */
TIM2_IRQn = 15, /*!< TIM2 Interrupt */
TIM3_IRQn = 16, /*!< TIM3 Interrupt */
TIM6_DAC_IRQn = 17, /*!< TIM6 and DAC Interrupts */
TIM14_IRQn = 19, /*!< TIM14 Interrupt */
TIM15_IRQn = 20, /*!< TIM15 Interrupt */
TIM16_IRQn = 21, /*!< TIM16 Interrupt */
TIM17_IRQn = 22, /*!< TIM17 Interrupt */
I2C1_IRQn = 23, /*!< I2C1 Interrupt */
I2C2_IRQn = 24, /*!< I2C2 Interrupt */
SPI1_IRQn = 25, /*!< SPI1 Interrupt */
SPI2_IRQn = 26, /*!< SPI2 Interrupt */
USART1_IRQn = 27, /*!< USART1 Interrupt */
USART2_IRQn = 28, /*!< USART2 Interrupt */
CEC_IRQn = 30 /*!< CEC Interrupt */
#elif defined (STM32F0XX_LD) || defined (STM32F030X6)
/****** STM32F0XX_LD and STM32F030X6 specific Interrupt Numbers *************************************/
WWDG_IRQn = 0, /*!< Window WatchDog Interrupt */
...
http://www.st.com/web/en/resource/technical/document/reference_manual/DM00091pdf
Interrupt and exception vectors, Table Vector tableUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-04 8:22 AM
Might want to review also ST's Cortex-M0 programming Manual
http://www.st.com/web/en/resource/technical/document/programming_manual/DM00051352.pdf
http://infocenter.arm.com/help/topic/com.arm.doc.ddi0432c/DDI0432C_cortex_m0_r0p0_trm.pdf
,http://www.amazon.com/The-Definitive-Guide-ARM-Cortex-M0/dp/0123854776
(s)Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-04 8:51 AM
Thanks
It is clear As per this table we can't manage every individual pin of each port. and we can only grouping pinsExample7 EXTI4_15 EXTI Line[15:4] interrupts- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-04 9:15 AM
As per this table we can't manage every individual pin of each port. and we can only grouping pins Example 7 EXTI4_15 EXTI Line[15:4] interrupts
But the peripheral will let you manage them. The core by design only supports 32 external sources, where external means outside the core, not the chip.Up vote any posts that you find helpful, it shows what's working..