2014-11-02 12:15 AM
Dear All
Following syntax does nit disable the global interruptPlease advice uint32_t PriMask = 0x01; //void __enable_irq (void);//Global Interrupt enable (using the instruction CPSIE i) void __set_PRIMASK (uint32_t PriMask );// M0, M3PRIMASK = value// Assign value to Priority Mask Register (usingthe instruction MSR) //void __disable_irq(void); //void __diasable_irq(void); //void __set_PRIMASK (uint32_t __set_PRIMASK); //uint32_t __get_PRIMASK(void)It is seem to be ''PRIMASK;bit does not disableplease advice how disable PRIMASK BIT disable with CMSIS source codeThanks in advance2014-11-08 08:37 PM