2007-09-30 2:10 PM
How can i use PA8 as MCO?
2011-05-17 3:16 AM
Dear wuguobing,
You can configure PA8 to MCO by simply calling these functions : /* Configure GPIOA ------------------------------------------*/ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA , ENABLE); /* Output HSE clock on MCO pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); RCC_MCOConfig(RCC_MCO_HSE); You can refer to the STM32 Firmware library using this link :http://www.st.com/stonline/products/support/micro/files/um0427.zip
Then you can go to the RCC Example in this directory ''STM32F10xFWLib/FWLib/examples/RCC'' where you will find more details ;) With best regards, STOne-322011-05-17 3:16 AM
PA8 is a multi-function pin, it's AF can be USART1_CK, TIM1_CH1 or MCO, how can i config it to be MCO?
I can remap TIM1 to none, but USART1_CK can't be remapped!2011-05-17 3:16 AM
Thanks a lot!
After reset, USART1_CK, TIM1_CH1 and MCO are disabled, to use PA8 as mco, just config MCO to work, and config PA8 to AF mode.:-D Only one AF on the same pin can be enabled. But if two AF functions in output mode is enabled at same time, what would happen, stm32 will be destroyed?