2020-02-19 1:35 AM
I am using CAN(MCP2515 Controller), I need to know the methods used to Test CAN Failure and Build in CAN Test.
Methods I tried. 1: Checking Error Flag like Bus-Off Error Flag bit and Passive Error Bit, but due to Arbitration Failure Transmit Error Counter is increasing and goes to Bus-Off. Arbitration Failure is not a CAN Failure so I don't want to consider that. So I need to know which Error is causing Bus-Off (Differentiate between Errors) but there is no Register on MCP2515 to show last error code.
If I want to Know the Last Error Status so I need to read Error message Frames(Removing Filters) that is not Compatible with my project.
Can you please suggest any idea and method I can Try. Thanks in Advance.
2020-02-19 2:06 AM
Is the bus termninated? can you communicate via CAN with other devices? Do you have a scope and/or a logic analyzer? Did you look with a scope on the can lines and with an logic anayzer? Yu need to check many things. And best is to start with a working setup and only exchange things step by step.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.