cancel
Showing results for 
Search instead for 
Did you mean: 

How can I detect when a 50 Hz signal is turned on and off, respectively?

arnold_w
Senior II

I am working with the STM32F446 microcontroller and I need to detect when a 50 Hz (plus-minus 2 Hz) square wave signal is turned on and off, respectively. The signal is connected to a pin that has TIMx_CHy alternate functionality. Is there a way to accomplish this without having to handle roughly 50 interrupts/second?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0