2013-03-09 5:40 AM
2013-03-09 6:21 AM
Is the result predictable? What is the expected output? What is the observed output?
2013-03-09 6:49 AM
2013-03-09 6:55 AM
i used this function as example you can find it on stm32F4xx_hash_sha1.c and it works fine i just need to transfer data to the hash possessor with dma (data are the key and the message to hash)
ErrorStatus HMAC_SHA1(uint8_t *Key, uint32_t Keylen, uint8_t *Input, uint32_t Ilen, uint8_t Output[20]){ HASH_InitTypeDef SHA1_HASH_InitStructure; HASH_MsgDigest SHA1_MessageDigest; __IO uint16_t nbvalidbitsdata = 0; __IO uint16_t nbvalidbitskey = 0; uint32_t i = 0; __IO uint32_t counter = 0; uint32_t busystatus = 0; ErrorStatus status = SUCCESS; uint32_t keyaddr = (uint32_t)Key; uint32_t inputaddr = (uint32_t)Input; uint32_t outputaddr = (uint32_t)Output; /* Number of valid bits in last word of the Input data */ nbvalidbitsdata = 8 * (Ilen % 4); /* Number of valid bits in last word of the Key */ nbvalidbitskey = 8 * (Keylen % 4); /* HASH peripheral initialization */ HASH_DeInit(); /* HASH Configuration */ SHA1_HASH_InitStructure.HASH_AlgoSelection = HASH_AlgoSelection_SHA1; SHA1_HASH_InitStructure.HASH_AlgoMode = HASH_AlgoMode_HMAC; SHA1_HASH_InitStructure.HASH_DataType = HASH_DataType_8b; if(Keylen > 64) { /* HMAC long Key */ SHA1_HASH_InitStructure.HASH_HMACKeyType = HASH_HMACKeyType_LongKey; } else { /* HMAC short Key */ SHA1_HASH_InitStructure.HASH_HMACKeyType = HASH_HMACKeyType_ShortKey; } HASH_Init(&SHA1_HASH_InitStructure); /* Configure the number of valid bits in last word of the Key */ HASH_SetLastWordValidBitsNbr(nbvalidbitskey); /* Write the Key */ for(i=0; i<Keylen; i+=4) { HASH_DataIn(*(uint32_t*)keyaddr); keyaddr+=4; } /* Start the HASH processor */ HASH_StartDigest(); /* wait until the Busy flag is RESET */ do { busystatus = HASH_GetFlagStatus(HASH_FLAG_BUSY); counter++; }while ((counter != SHA1BUSY_TIMEOUT) && (busystatus != RESET)); if (busystatus != RESET) { status = ERROR; } else { /* Configure the number of valid bits in last word of the Input data */ HASH_SetLastWordValidBitsNbr(nbvalidbitsdata); /* Write the Input block in the IN FIFO */ for(i=0; i<Ilen; i+=4) { HASH_DataIn(*(uint32_t*)inputaddr); inputaddr+=4; } /* Start the HASH processor */ HASH_StartDigest(); /* wait until the Busy flag is RESET */ counter =0; do { busystatus = HASH_GetFlagStatus(HASH_FLAG_BUSY); counter++; }while ((counter != SHA1BUSY_TIMEOUT) && (busystatus != RESET)); if (busystatus != RESET) { status = ERROR; } else { /* Configure the number of valid bits in last word of the Key */ HASH_SetLastWordValidBitsNbr(nbvalidbitskey); /* Write the Key */ keyaddr = (uint32_t)Key; for(i=0; i<Keylen; i+=4) { HASH_DataIn(*(uint32_t*)keyaddr); keyaddr+=4; } /* Start the HASH processor */ HASH_StartDigest(); /* wait until the Busy flag is RESET */ counter =0; do { busystatus = HASH_GetFlagStatus(HASH_FLAG_BUSY); counter++; }while ((counter != SHA1BUSY_TIMEOUT) && (busystatus != RESET)); if (busystatus != RESET) { status = ERROR; } else { /* Read the message digest */ HASH_GetDigest(&SHA1_MessageDigest); *(uint32_t*)(outputaddr) = __REV(SHA1_MessageDigest.Data[0]); outputaddr+=4; *(uint32_t*)(outputaddr) = __REV(SHA1_MessageDigest.Data[1]); outputaddr+=4; *(uint32_t*)(outputaddr) = __REV(SHA1_MessageDigest.Data[2]); outputaddr+=4; *(uint32_t*)(outputaddr) = __REV(SHA1_MessageDigest.Data[3]); outputaddr+=4; *(uint32_t*)(outputaddr) = __REV(SHA1_MessageDigest.Data[4]); } } } return status; }2013-03-09 8:01 AM
261 bytes, not 261 words = 261 x 4
The DMA count is in units, to do words the buffer must have such alignment, ie 261 is not divisible by 42013-03-09 10:24 AM
2013-03-09 1:38 PM
so im supposed to change the buffer to one with a size that is multiple of 4?
What I'm saying is you can't expect to hash data 32-bits at a time if you aren't working with integral lumps of 4 bytes. Using Word or HalfWord for a group of 261 bytes ain't going to work. Maybe you can decompose the transfer into runs which are optimal for different DMA transfer widths? Or course you might want to consider doing that with a scatter/gather list or chain under interrupt, rather than polling completion. 260 bytes would be 65 words (32-bit), and that would be the length programmed into the DMA controller for word transfers. I'd need to do a SHA1 of your original data to confirm the correct response, and the go dig up my F215 board to confirm the computation via the chip.2013-03-10 10:55 AM
Thank you clive i added 3 more bytes and it worked well
can i ask you an other favor??2013-03-10 11:14 AM
can i ask you an other favor??
Sure, if it can be asked in the form of a question.2013-03-10 11:26 AM
In my application i need to use the
Cryptographic processor (CRYP) some times to encrypt and other times to decrypt all this with the use of dma and with the minimum lost of time in the initialization i figured out that there’s only few differences between crypt and decrypt initialization but if change only the parameters that are deferent results come out corrupted .any idea to minimize the number of parameters to configure ???
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.