2013-03-09 5:40 AM
2013-03-10 11:33 AM
this is the code but i think that's too long to put it in an interruption
/*************************************************************************************//** * @brief Encrypt Data using AES * @note DATA transfer is done by the DMA * @note DMA2 stream6 channel2 is used to transfer data from memory (the * PlainData Table) to CRYP Peripheral (the INPUT data register). * @note DMA2 stream5 channel2 is used to transfer data from CRYP Peripheral * (the OUTPUT data register to memory (the EncryptedData Table). * @param None * @retval None ************************************************************************************/ void AES128_Encrypt_DMA_CBC(uint8_t* key, uint8_t* InitVectors){ uint32_t keyaddr = (uint32_t)key ; uint32_t ivaddr = (uint32_t)InitVectors; CRYP_IVInitTypeDef AES_CRYP_IVInitStructure ; CRYP_InitTypeDef CRYP_InitStructure ; CRYP_KeyInitTypeDef CRYP_KeyInitStructure ; CRYP_DeInit(); /* Enable CRYP clock */ RCC_AHB2PeriphClockCmd(RCC_AHB2Periph_CRYP, ENABLE); /* CRYP configuration********************************************************/ /* Crypto key structure initialisation */ CRYP_KeyStructInit(&CRYP_KeyInitStructure); CRYP_FIFOFlush(); /* Crypto Init for Encryption process */ CRYP_InitStructure.CRYP_AlgoDir = CRYP_AlgoDir_Encrypt; CRYP_InitStructure.CRYP_AlgoMode = CRYP_AlgoMode_AES_CBC; CRYP_InitStructure.CRYP_DataType = CRYP_DataType_8b; CRYP_InitStructure.CRYP_KeySize = CRYP_KeySize_128b; CRYP_Init(&CRYP_InitStructure); /* Key Initialisation ********************************************************/ CRYP_KeyInitStructure.CRYP_Key2Left = __REV(*(uint32_t*)(keyaddr));keyaddr+=4; CRYP_KeyInitStructure.CRYP_Key2Right= __REV(*(uint32_t*)(keyaddr));keyaddr+=4; CRYP_KeyInitStructure.CRYP_Key3Left = __REV(*(uint32_t*)(keyaddr));keyaddr+=4; CRYP_KeyInitStructure.CRYP_Key3Right= __REV(*(uint32_t*)(keyaddr)); CRYP_KeyInit(&CRYP_KeyInitStructure); /* CRYP Initialization Vectors **********************************************/ AES_CRYP_IVInitStructure.CRYP_IV0Left = __REV(*(uint32_t*)(ivaddr));ivaddr+=4; AES_CRYP_IVInitStructure.CRYP_IV0Right= __REV(*(uint32_t*)(ivaddr));ivaddr+=4; AES_CRYP_IVInitStructure.CRYP_IV1Left = __REV(*(uint32_t*)(ivaddr));ivaddr+=4; AES_CRYP_IVInitStructure.CRYP_IV1Right= __REV(*(uint32_t*)(ivaddr)); CRYP_IVInit(&AES_CRYP_IVInitStructure); /* Enable Crypto processor **************************************************/ CRYP_FIFOFlush(); CRYP_Cmd(ENABLE); CRYP_DMACmd(CRYP_DMAReq_DataIN, ENABLE); CRYP_DMACmd(CRYP_DMAReq_DataOUT, ENABLE);} /*********************** AES128_Decrypt_DMA_Configuration **************************//*************************************************************************************//** * @brief Decrypt Data using AES * @note DATA transfer is done by DMA * @note DMA2 stream6 channel2 is used to transfer data from memory (the * EncryptedData Table) to CRYP Peripheral (the INPUT data register). * @note DMA2 stream5 channel2 is used to transfer data from CRYP Peripheral * (the OUTPUT data register to memory (the DecryptedData Table). * @param None * @retval None ***********************************************************************************/void AES128_Decrypt_DMA_CBC(uint8_t* key, uint8_t* InitVectors){ uint32_t keyaddr = (uint32_t)key ; uint32_t ivaddr = (uint32_t)InitVectors; CRYP_IVInitTypeDef AES_CRYP_IVInitStructure; CRYP_InitTypeDef CRYP_InitStructure; CRYP_KeyInitTypeDef CRYP_KeyInitStructure;// CRYP_DeInit(); /* Enable CRYP clock */ RCC_AHB2PeriphClockCmd(RCC_AHB2Periph_CRYP, ENABLE); /* CRYP configuration*******************************************************/ /* Crypto Init for Key preparation for Decryption process */ CRYP_InitStructure.CRYP_AlgoDir = CRYP_AlgoDir_Decrypt; CRYP_InitStructure.CRYP_AlgoMode = CRYP_AlgoMode_AES_Key; CRYP_InitStructure.CRYP_DataType = CRYP_DataType_8b; CRYP_InitStructure.CRYP_KeySize = CRYP_KeySize_128b; CRYP_Init(&CRYP_InitStructure); /* Key Initialisation ******************************************************/ CRYP_KeyInitStructure.CRYP_Key2Left = __REV(*(uint32_t*)(keyaddr));keyaddr+=4; CRYP_KeyInitStructure.CRYP_Key2Right= __REV(*(uint32_t*)(keyaddr));keyaddr+=4; CRYP_KeyInitStructure.CRYP_Key3Left = __REV(*(uint32_t*)(keyaddr));keyaddr+=4; CRYP_KeyInitStructure.CRYP_Key3Right= __REV(*(uint32_t*)(keyaddr));keyaddr+=4; CRYP_KeyInit(&CRYP_KeyInitStructure); /* CRYP Initialization Vectors *********************************************/ AES_CRYP_IVInitStructure.CRYP_IV0Left = __REV(*(uint32_t*)(ivaddr));ivaddr+=4; AES_CRYP_IVInitStructure.CRYP_IV0Right= __REV(*(uint32_t*)(ivaddr));ivaddr+=4; AES_CRYP_IVInitStructure.CRYP_IV1Left = __REV(*(uint32_t*)(ivaddr));ivaddr+=4; AES_CRYP_IVInitStructure.CRYP_IV1Right= __REV(*(uint32_t*)(ivaddr)); CRYP_IVInit(&AES_CRYP_IVInitStructure); /* Enable Crypto processor */ CRYP_Cmd(ENABLE); /* wait until the Busy flag is reset */ while (CRYP_GetFlagStatus(CRYP_FLAG_BUSY) != RESET); /* Crypto Init for Decryption process */ CRYP_InitStructure.CRYP_AlgoDir = CRYP_AlgoDir_Decrypt; CRYP_InitStructure.CRYP_AlgoMode = CRYP_AlgoMode_AES_CBC; CRYP_InitStructure.CRYP_DataType = CRYP_DataType_8b; CRYP_InitStructure.CRYP_KeySize = CRYP_KeySize_128b; CRYP_Init(&CRYP_InitStructure); CRYP_Cmd(ENABLE); /* CRYP Initialization Vectors */ CRYP_DMACmd(CRYP_DMAReq_DataIN, ENABLE); CRYP_DMACmd(CRYP_DMAReq_DataOUT, ENABLE); }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.