2021-06-10 11:52 PM
2021-06-11 12:10 AM
Homework?
Run the timer so that it throws an interrupt each 0.1s, in that interrupt count individually for the three LEDs and toggle them accordingly.
JW
2021-06-11 12:23 AM
Hi,
Thanks for the reply.
I am new to this controller .Could you please explain it briefly. Or can you please give me the pseudocode as i am not getting how to count individually for 3 LEDS.
2021-06-11 1:40 AM
This has nothing to do with STM32, you would do it in the same way in any mcu.
Define a global variable
int led1counter;
then in the 0.1s interrupt or any other function periodically called at 0.1s period
if (led1counter == 40) { // 4.0s
Led1On();
} else if (led1counter == 40 + 3) { // after further 0.3s
Led1Off();
led1counter = 0; // restart
} else {
led1counter++;
}
and do the same for the remaining LEDs, with a different variable.
JW
2021-06-14 4:45 AM
2021-06-14 5:24 AM
> void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
> [...]
> timerValue = __HAL_TIM_GET_COUNTER(&htim3);
> [...]
This is nonsense, in the Update interrupt (which is what leads to HAL_TIM_PeriodElapsedCallback()), TIMx_CNT is always close to 0.
Do what I told you to do above.
JW
2021-06-14 6:22 AM
Here is an implementation like what JW suggests.
1. Grab a periodic interrupt, either set up a 10Hz/100msec timer in MX, or piggyback on an existing.
I'm piggybacking on the 1KHz as I have things I need checked at 1msec.
//stm32f4xx_it.c (or equivalent depending on which MCU is used): we need to call our system timer callback in the SysTick_Handler() function (around line 186).
//The function should now look like this:
//This function handles System tick timer.
void SysTick_Handler(void)
{
/* USER CODE BEGIN SysTick_IRQn 0 */
/* USER CODE END SysTick_IRQn 0 */
HAL_IncTick();
/* USER CODE BEGIN SysTick_IRQn 1 */
void vTmrCallbackMy1KHz(void); vTmrCallbackMy1KHz();
/* USER CODE END SysTick_IRQn 1 */
}2. Write your own vTmrCallbackMy1KHz() (or whatever you called it)
This is very simple implementation.
In a real project I might use callbacks for critical timing events (not blinking a LED so slowly).
I'd also use functions to check the bools, good coding style is to NOT make them global
You could also blink the LEDs directly in the function below using the LED's matching Toggle call, but I prefer a bool incase LED is also following another signal for whether On/Off/blinking, or an enum for On/BlinkFast/BlinkSlow/Off.
bool b4000msec;
bool b300msec;
bool b700msec;
bool b4700msec;
void vTmrCallbackMy1KHz(void)
{
static uint32_t uCount4000msec;
static uint32_t uCount300msec;
static uint32_t uCount700msec;
static uint32_t uCount4700msec;
if (++uCount4000msec >=4000){uCount4000msec =0; b4000msec=true;}
if (++uCount300msec>=300){uCount300msec=0; b300msec=true;}
if (++uCount700msec>=700){uCount700msec=0; b700msec=true;}
if (++uCount4700msec>=4700){uCount4700msec=0; b4700msec=true;}
}Paul