2020-07-20 3:36 AM
can anyone help me with the code ....thanks in advance
here is my code
static void MX_CAN1_Init(void)
{
/* USER CODE BEGIN CAN1_Init 0 */
/* USER CODE END CAN1_Init 0 */
/* USER CODE BEGIN CAN1_Init 1 */
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 30;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_15TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init 2 */
/* USER CODE END CAN1_Init 2 */
}
/**
* @brief CAN2 Initialization Function
* @param None
* @retval None
*/
static void MX_CAN2_Init(void)
{
/* USER CODE BEGIN CAN2_Init 0 */
/* USER CODE END CAN2_Init 0 */
/* USER CODE BEGIN CAN2_Init 1 */
/* USER CODE END CAN2_Init 1 */
hcan2.Instance = CAN2;
hcan2.Init.Prescaler = 30;
hcan2.Init.Mode = CAN_MODE_NORMAL;
hcan2.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan2.Init.TimeSeg1 = CAN_BS1_15TQ;
hcan2.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan2.Init.TimeTriggeredMode = DISABLE;
hcan2.Init.AutoBusOff = DISABLE;
hcan2.Init.AutoWakeUp = DISABLE;
hcan2.Init.AutoRetransmission = DISABLE;
hcan2.Init.ReceiveFifoLocked = DISABLE;
hcan2.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN2_Init 2 */
/* USER CODE END CAN2_Init 2 */
}
void can1_filter(void)
{
CAN_FilterTypeDef filter1;
filter1.FilterActivation=CAN_FILTER_ENABLE;
filter1.FilterBank=0;
filter1.FilterFIFOAssignment=CAN_RX_FIFO0;
filter1.FilterIdHigh=0x0000;
filter1.FilterIdLow=0x0000;
filter1.FilterMaskIdHigh=0x0000;
filter1.FilterMaskIdLow=0x0000;
filter1.FilterMode= CAN_FILTERMODE_IDMASK;
filter1.FilterScale=CAN_FILTERSCALE_32BIT;
filter1.SlaveStartFilterBank=13;
if(HAL_CAN_ConfigFilter(&hcan1,&filter1)!=HAL_OK)
{
Error_Handler();
}
}
void can2_filter(void)
{
CAN_FilterTypeDef filter2;
filter2.FilterActivation=CAN_FILTER_ENABLE;
filter2.FilterBank=0;
filter2.FilterFIFOAssignment= CAN_RX_FIFO0;
filter2.FilterIdHigh=0x0000;
filter2.FilterIdLow=0x0000;
filter2.FilterMaskIdHigh=0x0000;
filter2.FilterMaskIdLow=0x0000;
filter2.FilterMode= CAN_FILTERMODE_IDMASK;
filter2.FilterScale=CAN_FILTERSCALE_32BIT;
filter2.SlaveStartFilterBank=14;
if(HAL_CAN_ConfigFilter(&hcan2,&filter2)!=HAL_OK)
{
Error_Handler();
}
}
void can(void)
{
CAN_TxHeaderTypeDef TxHeader;
uint32_t TxMailbox;
uint8_t usr_msg[8];
usr_msg[0]=0xAF;
//usr_msg[1]=0xAD;
TxHeader.DLC=2;
TxHeader.RTR= CAN_RTR_DATA ;
TxHeader.IDE= CAN_ID_STD;
TxHeader.StdId= 0x65;
if(HAL_CAN_AddTxMessage(&hcan1,&TxHeader,usr_msg,&TxMailbox)!=HAL_OK)
{
Error_Handler();
}
while(HAL_CAN_IsTxMessagePending(&hcan1,TxMailbox));
HAL_GPIO_WritePin(GPIOB, LD1_Pin, GPIO_PIN_SET);
}
void RX(void)
{
CAN_RxHeaderTypeDef RxHeader;
uint8_t rcv_msg[10];
while(HAL_CAN_GetRxFifoFillLevel(&hcan2,CAN_RX_FIFO0)<1);
if(HAL_CAN_GetRxMessage(&hcan2,CAN_RX_FIFO0,&RxHeader,rcv_msg)!=HAL_OK)
{
//HAL_CAN_GetError(&hcan2);
Error_Handler();
}
HAL_GPIO_WritePin(GPIOB, LD2_Pin, GPIO_PIN_SET);
}