2021-02-28 04:30 PM
2021-02-28 04:57 PM
If you have already googled and tried all the advises, I don't know what else can help.
-- pa
2021-02-28 05:10 PM
i have implemented the tool settings adding -u float in the C linker settings not any other solution.
2021-02-28 10:29 PM
There should a a documentation of the libraries available.
Check those if they support float formats for printf-like functions. Some do not, for size reasons.
The F1 are M3 controllers without FPU, I would consider integer-based algorithms.