cancel
Showing results for 
Search instead for 
Did you mean: 

Hi eveyone, i am using stm32f207zg and i want to do a multi channel conversion with adc1. The input pin are PA5 e PA6. The problem is when i play the program: in particulare using debug i note that adc doesn't conversion as the sequence is defined.

FCa.1
Associate II

int main(void){

double digital;

char Stringa[20];  

int x=1,k,j,i=0;

RCC_CFGR=RCC_CFGR|0xE000;   //clock divided by 16---->APB2 pheripherals CLK = 1MHz

RCC_APB1ENR=RCC_APB1ENR|0x20001;    //abilitazione clock per TIMER2 e USART2

RCC_CR=RCC_CR|0x1;   

RCC_APB2ENR=0x101;          //abilitazione clock per TIMER1 e ADC1

RCC_AHB1ENR=0x40000F;        //abilitazione clock GPIOA, GPIOB,GPIOC e GPIOD e DMA2

GPIOB_MODER=0x10004001;  

GPIOA_MODER=GPIOA_MODER|0x2BC00;  //pin A7,A8 in alternate function mode e pin A6 e A5 in analog mode

GPIOD_MODER=0x2800;         //pin D5/D6 in alternate function mode

GPIOD_AFRL=GPIOD_AFRL|0x7700000;  //mappo PD5/PD6 per USART2

//NVIC_ADC=0x40000;

DMA2_S0PAR=0x4001204C;   //base address della periferica dalla quale lo stream prende il dato

DMA2_S0M0AR=0x40020814;  //indirizzo di memoria dove scrivere il dato

DMA2_S0NDTR=DMA2_S0NDTR|0xFFFF; //numero di elementi da trasferire

//DMA2_S0CR=DMA2_S0CR|0x400;

DMA2_S0CR=DMA2_S0CR|0x75111;  //stream enabled, DIR, circular mode e interrupt enabled

ADC1_CR1=ADC1_CR1|0x100;  //Scan mode enabled 

ADC1_SQR1=0x100000; //regular sequence lenght

ADC1_SQR3=0xC5;  //canale 5(PA5) come primo nella sequenza e PA6 come secondo nella sequenza

ADC1_SMPR2=0x1D8000;  //56 cycles per entrambi i canali

ADC1_CR2=ADC1_CR2|0x503;  //ADC ON, continuos conversion mode DMA mode enabled

 TIM2_CNT=0x0;

 TIM2_ARR=0x1E8;  //intervallo di conteggio pari a 10ms

  USART2_BRR=0x8B; //fisso un baud rate pari a 115200 simb/s

  USART2_CR1=USART2_CR1|0x200C;  //transmit e receiver enable e usart enable

ADC1_CR2=ADC1_CR2|0x40000000; //avvio della conversione

digital=GPIOC_ODR;

}

For example, playing the program, it converts ch5 for a certain time(casual) then convert ch6 but it doesn't convert the channel alternately.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0