2013-03-04 9:09 AM
Hi guys. First of all, sorry if my english is bad.
I have a problem configuring a uSD and SDIO port. I'm using the ST SDIO example for STM32f4 discovery board and I cant comunicate with de micro SD. I checked the pins config, clock speed and everything seems to be ok. But if I check the pins voltaje, all are at 3v (by the pull ups resistors) and the clock is at 0v always.When I see the clock signal with my oscilloscope I can see it never starts. So I get a SD_CMD_RSP_TIMEOUT from CmdError().Here is the code./**************************************************/int main(void){ /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup file (startup_stm32f4xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f4xx.c file */ /* Interrupt Config */ NVIC_Configuration(); /*------------------------------ SD Init ---------------------------------- */ if ((Status = SD_Init()) != SD_OK) { STM_EVAL_LEDOn(LED6); // Error LED } [...]while(1);}/**************************************************/SD_Error SD_Init(void) { __IO SD_Error errorstatus = SD_OK; /* SDIO Peripheral Low Level Init */ SD_LowLevel_Init(); errorstatus = SD_PowerON(); if (errorstatus != SD_OK) { /*!< CMD Response TimeOut (wait for CMDSENT flag) */ return (errorstatus); [...]}/*******************************************/void SD_LowLevel_Init(void){ GPIO_InitTypeDef GPIO_InitStructure; /* GPIOC and GPIOD Periph clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOD | SD_DETECT_GPIO_CLK, ENABLE); /* Configure PC.08, PC.09, PC.10, PC.11 pins: D0, D1, D2, D3 pins */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOC, GPIO_PinSource8, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_SDIO); /* Configure PD.02 CMD line */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_Init(GPIOD, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOD, GPIO_PinSource2, GPIO_AF_SDIO); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOD, &GPIO_InitStructure); /* Configure PC.12 pin: CLK pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure); /*!< Configure SD_SPI_DETECT_PIN pin: SD Card detect pin */ GPIO_InitStructure.GPIO_Pin = SD_DETECT_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(SD_DETECT_GPIO_PORT, &GPIO_InitStructure); /* Enable the SDIO APB2 Clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SDIO, ENABLE); /* Enable the DMA2 Clock */ RCC_AHB1PeriphClockCmd(SD_SDIO_DMA_CLK, ENABLE); SDIO_SetPowerState(SDIO_PowerState_ON); SDIO_ClockCmd(ENABLE);}/*******************************************/SD_Error SD_PowerON(void) { __IO SD_Error errorstatus = SD_OK; uint32_t response = 0, count = 0, validvoltage = 0; uint32_t SDType = SD_STD_CAPACITY; /*!< Power ON Sequence -----------------------------------------------------*/ /*!< Configure the SDIO peripheral */ /*!< SDIO_CK = SDIOCLK / (SDIO_INIT_CLK_DIV + 2) */ /*!< on STM32F4xx devices, SDIOCLK is fixed to 48MHz */ /*!< SDIO_CK for initialization should not exceed 400 KHz */ SDIO_InitStructure.SDIO_ClockDiv = 120; //SDIO_INIT_CLK_DIV; SDIO_InitStructure.SDIO_ClockEdge = SDIO_ClockEdge_Rising; SDIO_InitStructure.SDIO_ClockBypass = SDIO_ClockBypass_Disable; SDIO_InitStructure.SDIO_ClockPowerSave = SDIO_ClockPowerSave_Disable; SDIO_InitStructure.SDIO_BusWide = SDIO_BusWide_4b; SDIO_InitStructure.SDIO_HardwareFlowControl = SDIO_HardwareFlowControl_Disable; SDIO_Init(&SDIO_InitStructure); /*!< Set Power State to ON */ SDIO_SetPowerState(SDIO_PowerState_ON); /*!< Enable SDIO Clock */ SDIO_ClockCmd(ENABLE); /*!< CMD0: GO_IDLE_STATE ---------------------------------------------------*/ /*!< No CMD response required */ SDIO_CmdInitStructure.SDIO_Argument = 0x0; SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_GO_IDLE_STATE; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_No; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure); errorstatus = CmdError(); if (errorstatus != SD_OK) { /*!< CMD Response TimeOut (wait for CMDSENT flag) */ return (errorstatus); }/*******************************************/As you can see I only paste the parts of the code that my system execute.Please, help me! #sdcard-stm32f4-sdio-fatfs2013-03-04 9:46 AM
The nonsense with PD12..15 causes you to misconfigure the clock pin.
Also setting the slew rate to 2 MHz probably isn't where you want to be when running the SDIO at 24 MHz. I've previously posted working code to attach an MicroSD card to the STM32F4-Discovery and use FatFs2013-03-04 10:08 AM
Thanks for you reply!
Same Error with your example =/. And the clock pin still at 0v.Any idea what's happening or what could be the error?regards2013-03-06 8:23 AM
Solved!
I forgot to add SystemInit() before main() in Startup_stm32f4xx.cThanks!2013-07-11 6:17 AM
2013-09-12 3:01 AM
2013-09-14 5:03 AM
I wait your reply. Where is your reply??
2013-09-14 3:14 PM
I wait your reply. Where is your reply??
Perhaps no one currently browsing the forum has a logic analyzer attached to the SDIO bus? I guess if I wanted to observe SDIO bus traffic, I'd just use the example code from the firmware library and have it do block reads in a loop.