cancel
Showing results for 
Search instead for 
Did you mean: 

Help with Dual ADC simultaneous, No DMA, ADC1 with 2 injected channels, ADC 2 with 2 injected channels

ATo
Associate II

I need to have ADC1 and ADC2 run sumultaneously. Each ADC has 2 injected channels. I want to start the ADC once and then have it constantly run converting the 4 injected channels, putting the result in the 4 associated JDR registers and raising a flag in the ADC conversion complete interrupt to tell my main program that data is available for me to read from the 4 JDR registers.

Is that possible, if so can someone kindly provide example code?

The ADC on this uC is so complicated, I can not make heads or tails of anything.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Bowman32
ST Employee

Hello @ATo​ 

Please refer to Injected simultaneous mode in STM32H7 reference manuel RM0433 Rev 7.

Best regards

Bouraoui