2024-12-17 11:27 AM
Hi,
I am a newbie with STM32. I need help.
I want to configure that PA15 pin (which by default is used as JTDI), as a GPIO output.
I've added the following two lines to the beginning of the generated code of MX_GPIO_Init():
LL_GPIO_SetAFPin_8_15(GPIOA,LL_GPIO_PIN_15,LL_GPIO_AF_5);
LL_GPIO_SetPinMode(GPIOA,LL_GPIO_PIN_15,LL_GPIO_MODE_OUTPUT);
But it does not work. I connected a LED and tried to change the state of the pin high and low,
but it did not work.
I appreciate if someone help me to figure out what I am missing.
Thanks
Solved! Go to Solution.
2024-12-25 10:20 PM
Thanks a lot Karl and gbm.
You solved my issue.
Happy new year
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.