Help to interface AT24C256 EEPROM with STM32F051r8
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-07 8:42 AM
I am trying to to write/read to at24c256.
Iam new to I2C.
I read about all theory stuffs.
But i tried writing code from the i2c eeprom eg, but am not to able to skip the txis flag while loop.
Please help.
I commented the data write and all..not even the first line works and generates a acknowledgment. Have i missed some initialization functions?
/* Includes ------------------------------------------------------------------*/
#include 'main.h'#include 'stm32f0xx_rcc.h'#include 'stm32f0xx_gpio.h'#include 'stm32f0xx_i2c.h'/** @addtogroup STM32F0xx_StdPeriph_Templates * @{ *//* Private typedef -----------------------------------------------------------*/
#define EEPROM_ADDRESS 0x50#define sEE_WRITE_ADDRESS1 0x01/* Private define ------------------------------------------------------------*//* Private macro -------------------------------------------------------------*//* Private variables ---------------------------------------------------------*//* Private function prototypes -----------------------------------------------*//* Private functions ---------------------------------------------------------*//**
* @brief Main program. * @param None * @retval None */int main(void){/*!< At this stage the microcontroller clock setting is already configured,
this is done through SystemInit() function which is called from startup file (startup_stm32f0xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f0xx.c file */ /* Add your application code here *///clocks enable RCC_I2CCLKConfig(RCC_I2C1CLK_HSI); RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2,ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB,ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,ENABLE); GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_1;GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;GPIO_Init(GPIOC,&GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_1;GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;GPIO_Init(GPIOC,&GPIO_InitStructure); I2C_DeInit(I2C2); GPIO_InitTypeDef I2C_GPIO_CONGIG; I2C_GPIO_CONGIG.GPIO_Pin=GPIO_Pin_10; I2C_GPIO_CONGIG.GPIO_Mode=GPIO_Mode_AF; I2C_GPIO_CONGIG.GPIO_OType=GPIO_OType_OD; I2C_GPIO_CONGIG.GPIO_PuPd=GPIO_PuPd_NOPULL; I2C_GPIO_CONGIG.GPIO_Speed=GPIO_Speed_2MHz; GPIO_Init(GPIOB,&I2C_GPIO_CONGIG); //SCL I2C_GPIO_CONGIG.GPIO_Pin=GPIO_Pin_11; GPIO_Init(GPIOB,&I2C_GPIO_CONGIG); //SDA GPIO_PinAFConfig(GPIOB,GPIO_Pin_10,GPIO_AF_1); GPIO_PinAFConfig(GPIOB,GPIO_Pin_11,GPIO_AF_1); //I2C config I2C_InitTypeDef I2C_InitStructure; I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Enable; I2C_InitStructure.I2C_DigitalFilter = 0x00; I2C_InitStructure.I2C_OwnAddress1 = 0x00; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_Timing = 0x00201D2B; // I2C_InitStructure.I2C_Timing = 0x1042C3C7; I2C_Init(I2C2,&I2C_InitStructure); //I2c enable I2C_Cmd(I2C2,ENABLE); while(I2C_GetFlagStatus(I2C2, I2C_FLAG_BUSY) == SET) {} I2C_TransferHandling(I2C2,EEPROM_ADDRESS,1,I2C_Reload_Mode,I2C_Generate_Start_Write); /* Infinite loop */ while(I2C_GetFlagStatus(I2C2, I2C_ISR_TXIS) == RESET) { GPIO_WriteBit(GPIOC,GPIO_Pin_9,Bit_SET); } GPIO_WriteBit(GPIOC,GPIO_Pin_9,Bit_RESET); I2C_SendData(I2C2, 0x00);GPIO_WriteBit(GPIOC,GPIO_Pin_8,Bit_SET);
//Ensure that the transfer complete reload flag is //set, essentially a standard TC flag while(I2C_GetFlagStatus(I2C2, I2C_FLAG_TCR) == RESET){}// // // // /* Send MSB of memory address */// I2C_SendData(sEE_I2C, (uint8_t)((sEE_WRITE_ADDRESS1 & 0xFF00) >> 8)); // // while(I2C_GetFlagStatus(sEE_I2C, I2C_ISR_TXIS) == RESET)// {// // GPIO_WriteBit(GPIOC,GPIO_Pin_8,Bit_SET);// // }// // // // I2C_SendData(sEE_I2C, (uint8_t)(sEE_WRITE_ADDRESS1 & 0x00FF));// // while(I2C_GetFlagStatus(sEE_I2C, I2C_ISR_TCR) == RESET)// {// } while (1) {}
}#ifdef USE_FULL_ASSERT/**
* @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* User can add his own implementation to report the file name and line number, ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) *//* Infinite loop */
while (1) { }}#endif/**
* @} *//************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-07 4:03 PM
do you have a nucleo board?
can you try some examples first, see how they work.
The cube has many examples, there should be one for your processor and IIC.
IOt is a very steep learning curve after 3 years you become self reliant
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-07 4:24 PM
GPIO_PinAFConfig(GPIOB,GPIO_PinSource10,GPIO_AF_1); // Use PinSource index for AF config
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
‎2018-04-07 8:08 PM
This is not a direct answer, but if you picked up an mbed compatible nucleo or disco board you could get this running in a couple minutes. I've used this eeprom library with 24Cxx chips before with great success.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-07 10:54 PM
I dont have . got only stm32f051 discovery board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-07 10:55 PM
woww..thankyou...i never noticed that....You think it makes a differenc??Let me try and tell you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-07 10:56 PM
I dont wont entire library function. I want to learn.. So i need to use basic I2C function and do it
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-07 11:02 PM
Here is a hint from Vasile,
If you use HAL, look here
/external-link.jspa?url=http%3A%2F%2Fstm32f4-discovery.net%2F2015%2F07%2Fhal-library-16-i2c-for-stm32fxxx-devices%2F
If you use SPL, look here
/external-link.jspa?url=http%3A%2F%2Fstm32f4-discovery.net%2F2014%2F05%2Flibrary-09-i2c-for-stm32f4xx%2F