2007-11-27 04:03 AM
HELP: FLASH problerms
2011-05-17 03:18 AM
Hello ,everyone.
I am a novice in flash use. I plan to use a 2M flash to store my data , then FPGA read the data written in the flash. The problem is what tools and software i need to use? How about using jtag to download the data sheet.How could I write the data into the flash? Can someone help me? Thanks very much.2011-05-17 03:18 AM
Dear hapyang204,
I think that you are not the suitable forum discussion: Here is about STM32 32-bits Microcontrollers from ST and not NOR Flash , for more details refer to . :-o Regards, STOne-32