cancel
Showing results for 
Search instead for 
Did you mean: 

HELP: FLASH problerms

hapyang204
Associate II
Posted on November 27, 2007 at 13:03

HELP: FLASH problerms

2 REPLIES 2
hapyang204
Associate II
Posted on May 17, 2011 at 12:18

Hello ,everyone.

I am a novice in flash use.

I plan to use a 2M flash to store my data , then FPGA read the data written in the flash. The problem is what tools and software i need to use? How about using jtag to download the data sheet.How could I write the data into the flash?

Can someone help me? Thanks very much.

16-32micros
Associate III
Posted on May 17, 2011 at 12:18

Dear hapyang204,

I think that you are not the suitable forum discussion: Here is about STM32 32-bits Microcontrollers from ST and not NOR Flash , for more details refer to

http://www.st.com/stm32

. :o

Regards, STOne-32