2022-05-03 12:51 AM
2022-05-03 3:39 AM
Welcome, @AAAZO.1, to the community!
The HSE can only be used if:
Does it answer your question?
Regards
/Peter
2022-05-03 4:34 AM
On a Nucleo board the HSE clock can come from the STLINK, if it is not populated with a crystal.
But you have to consult the schematics of the board, on some Nucleo there is a solder bridge to add for this functionality.