cancel
Showing results for 
Search instead for 
Did you mean: 

Has issue on a project to use FileX to access SD card on stm32f429zi Nucleo board

XZhu.3
Associate II

Project name: Fx_MultiAcess_429

Type: STM32CubeIDE project

MCU/board: stm32f429zi Nucleo board

Purpose: This project uses FileX to access SD card on stm32f429zi Nucleo board (board version:MB1137-F429ZI-B01)

board pin connections(CN8 connector) vs SD Card Slot Socket pin:

PC8 -- SDIO-D0

PC9 -- SDIO-D1

PC10 -- SDIO-D2

PC11 -- SDIO-D3

PC12 -- SDIO-CK

PD2 -- SDIO-CMD

+3.3 -- +3.3

GND -- GND

I created this project thru clone from sample project "Fx_MultiAcess" on stm32f469 Discovery Board.

1. generated base codes thru IOC file by compareing screenshots of IOC file on project "Fx_MultiAcess" on stm32f469 Discovery Board;

2. copied app_file.c from project "Fx_MultiAcess" on stm32f469 Discovery Board;

3. added USART3 debug print out in main.c and app_file.c.

4. BTW, there is a small bug on sample project "Fx_MultiAcess" on stm32f469 Discovery Board. after regenerate codes thru IOC, 

line 199 of main.c has been set to "hsd.Init.BusWide = SDIO_BUS_WIDE_4B;"(not good) instead of "hsd.Init.BusWide = SDIO_BUS_WIDE_1B;"(good)  

The SD Card itself is good and has been verified thru running the above sample project on the stm32f469 Discovery Board.

Issues: 

Has error on line 191 of app_filex.c. fx_media_open() returns 0x01 (Error reading the media's boot sector)

Hope someone or ST team can help to find out why.

attached is the project file. 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
XZhu.3
Associate II

I have some new finding regarding the SD clock settings between stm32f469 and stm32f429. it may cause the SD function is not working on 429.

Please see the attached pic.

Hope a ST employee can answer the Q.

XZhu.3
Associate II

still, nobody answers!