cancel
Showing results for 
Search instead for 
Did you mean: 

Hardware details required for ADC example

ramadevi
Associate II
Posted on April 06, 2010 at 08:59

Hardware details required for ADC example

3 REPLIES 3
ramadevi
Associate II
Posted on May 17, 2011 at 13:46

Dear STM32One,

Could you please help me?

Posted on May 17, 2011 at 13:46

As already explained to you on the Keil forum, this is clearly shown in the schematics!

http://www.keil.com/forum/docs/thread16660.asp

(note that there are additional replies in that thread since your last post there)

ramadevi
Associate II
Posted on May 17, 2011 at 13:46

I think I failed to explain my doubt.Yes, I have seen the responses at Keil.

From the schematics, I could understand that the pin PC4 in Extension connector is connected to the on-board pot RV1. I

I was confused where to connect the variable power supply leads.Because I were able to see values changing for the ADCConvertedValue without connecting variable supply to PC4 and POT not being adjusted.Also when I tested the pins PC4 and GND with a multimeter with POT varying, the voltage goes to 0-3.26V.How then the external supply helps?

I am novice to this kind of activity and am learning the basics of microcontrollers.