Hard Fault when calling the HAL_TIM_Encoder_Start_DMA function on the STM32F103C8T6 microcontroller. Can I fix it?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-02 6:53 AM
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_CAN_Init();
MX_USART2_UART_Init();
MX_TIM3_Init();
MX_TIM4_Init();
MX_ADC1_Init();
MX_USART3_UART_Init();
MX_TIM2_Init();
HAL_ADC_Start_DMA(&hadc1,(uint32_t*) &ADC_Data,2);
HAL_TIM_Base_Start(&htim3);
HAL_TIM_Encoder_Start_DMA(&htim3, TIM_CHANNEL_ALL, tim3CH1, tim3CH2, 8);
HAL_TIM_Base_Start(&htim4);
HAL_TIM_Encoder_Start_DMA(&htim4, TIM_CHANNEL_ALL, tim3CH1, tim3CH2, 8);
/////////////////////////////////////////////////////
in function HAL_TIM_Encoder_Start_DMA(&htim3, TIM_CHANNEL_ALL, tim3CH1, tim3CH2, 8);
stm32f1xx_hal_tim.c
3046 htim->hdma[TIM_DMA_ID_CC1]->XferHalfCpltCallback = TIM_DMACaptureHalfCplt;
///////////////////////////////////////////////////
in disassembly
3046 htim->hdma[TIM_DMA_ID_CC1]->XferHalfCpltCallback = TIM_DMACaptureHalfCplt;
08003fd4: ldr r3, [r7, #12]
08003fd6: ldr r3, [r3, #36] ; 0x24
08003fd8: ldr r2, [pc, #176] ; (0x800408c <HAL_TIM_Encoder_Start_DMA+484>)
08003fda: str r2, [r3, #44] ; 0x2c
/////////////////////////////////////////////////
ldr r3, [r7, #12]
r7 = 0x20004fd0
Failed to execute MI command:
-data-disassemble -s 536891345 -e 536891509 -- 3
Error message from debugger back end:
Cannot access memory at address 0x20005000
- Labels:
-
STM32F1 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-02 10:56 AM
Blue Pill?
Genuine STM32?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-02 11:14 AM
Yeap, well your going to have to dig more. Perhaps have a better Hard Fault Handler, and review the code around the fault with much more context.
Check stack and heap.
Check structures, and pointers.
Make sure structures are cleared and setup properly. Especially auto/local ones.
Make sure DMA/IRQ related structures are in scope, and not auto/local variables.
Make sure all IRQ Handlers and Callbacks are present.
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
‎2020-03-02 9:37 PM
Yes, this is a blue tablet, but the marking from the ST is written on the chip.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-02 11:13 PM
> marking from the ST is written on the chip
This unfortunately is no guarantee. There are many counterfeits around - some are genuine ST chips but relabelled for a higher capacity (e.g. https://github.com/keirf/Greaseweazle/wiki/STM32-Fakes ) ; some are other manufacturer's clones, sometimes also relabelled as ST's (e.g. https://www.richis-lab.de/STM32_04.htm ).
I don't say this *is* the case with your board, and the problem may be elsewhere - see Clive's post above. But if you are starting with STM32, you may be better off buying a - possibly more expensive - board with a guarantee that it will work - maybe a Nucleo board, which comes also with an on-board STLink.
Btw. the STM32F1xx family was the first STM32, is more than 10 years old and - again from the point of view of a novice - using some of its facilities is harder than with some of the newer families.
JW