Skip to main content
Associate III
May 20, 2024 7:19 AM UTC
Solved

Hard fault handler

Hello,

I am using the STM32U575ZIT6 microcontroller and enabling the TrustZone option. When executing projects, the HardFault handler triggers when switching to the non-secure zone, displaying the message "No source available for <signal handler called>() at 0xffffffa9". This also happens when running a blank project. Do you have any solutions?

This topic has been closed for replies.
IstillagaBest answer
Associate III
May 20, 2024 2:17 PM UTC

Hello,

I have managed to resolve the issue. The error was that the values of AttributeConfig.MPCBB_SecConfig_array when initializing GTZC were set to 0xFFFFFFFF when they should have been 0x00000000.

1 reply

IstillagaAuthorBest answer
Associate III
May 20, 2024 2:17 PM UTC

Hello,

I have managed to resolve the issue. The error was that the values of AttributeConfig.MPCBB_SecConfig_array when initializing GTZC were set to 0xFFFFFFFF when they should have been 0x00000000.