2025-08-17 2:33 PM
Hi,
I'm using a STM32L031. When I'm entering the low power sleep mode und an interrupt occurs i'm getting a hard fault. The programm counter from the stack frame has ether the value 0x00000000 or is pointing at the __ISB after the __WFI - depending on the version i'm using. At the beginning i was using Enter_LP_Sleep1() getting 0x00000000. Then i found a blog discussion where they described the entering procedure of version Enter_LP_Sleep2(). This worked for my project and i thought the problem was solved. Unfortunately every now and then i got the problem with the hard fault again (depending on temperature?!). Now I stripped the code down to the following where i always get the hard fault.
int main(void){
FLASH->ACR |= FLASH_ACR_PRFTEN;
RCC->APB2ENR |= RCC_APB2ENR_SYSCFGEN;
RCC->APB1ENR |= RCC_APB1ENR_PWREN;
RCC->APB1SMENR = 0;
RCC->APB2SMENR = 0;
RCC->APB2SMENR |= RCC_APB2SMENR_TIM22SMEN;
RCC->APB1SMENR |= RCC_APB1SMENR_PWRSMEN;
RCC->APB2SMENR |= RCC_APB2SMENR_SYSCFGSMEN;
RCC->APB2SMENR |= RCC_APB2SMENR_DBGSMEN;
RCC->APB1SMENR |= RCC_APB1SMENR_LPTIM1SMEN;
RCC->APB1SMENR |= RCC_APB1SMENR_WWDGSMEN;
RCC->CSR |= RCC_CSR_LSION;
while(!(RCC->CSR & RCC_CSR_LSIRDY));
RCC->CCIPR |= RCC_CCIPR_LPTIM1SEL_0;
RCC->APB1ENR |= RCC_APB1ENR_LPTIM1EN;
NVIC_EnableIRQ(LPTIM1_IRQn);
NVIC_SetPriority(LPTIM1_IRQn, 3);
LPTIM1->CFGR |= 0b101 << 9;
LPTIM1->IER |= 0b11;
LPTIM1->CR |= LPTIM_CR_ENABLE;
LPTIM1->ARR = (1156.25 / 1000)*(1500);
LPTIM1->CMP = (1156.25 / 1000)*1000;
LPTIM1->CR |= LPTIM_CR_SNGSTRT;
Enter_LP_Sleep1(); // or Enter_LP_Sleep2();
while(1);
}
void Enter_LP_Sleep1(){
SCB->SCR &= ~SCB_SCR_SLEEPDEEP_Msk;
FLASH->ACR &= ~FLASH_ACR_SLEEP_PD;
PWR->CR &= ~PWR_CR_ULP;
PWR->CR |= PWR_CR_CWUF;
while (FLASH->SR & FLASH_SR_BSY) {}
PWR->CR |= PWR_CR_LPSDSR;
__WFI();
status_blockade = 0;
}
void Enter_LP_Sleep2(){
SCB->SCR &= ~SCB_SCR_SLEEPDEEP_Msk;
FLASH->ACR &= ~FLASH_ACR_SLEEP_PD;
PWR->CR &= ~PWR_CR_ULP;
PWR->CR |= PWR_CR_CWUF;
while (FLASH->SR & FLASH_SR_BSY) {}
PWR->CR |= PWR_CR_LPSDSR;
__disable_irq();
__DSB();
__WFI();
asm ("nop");
__ISB();
__enable_irq();
status_blockade = 0;
}Thanks in advance!
Greetings from Salzburg / Austria
2025-08-19 10:56 PM
To be honest, I mostly dealt with M3 and higher in this regard.
Perhaps this can help you : https://community.arm.com/support-forums/f/embedded-and-microcontrollers-forum/3257/debugging-a-cortex-m0-hard-fault
2025-08-19 11:03 PM
Thanks for the link - i alteady read this but it didn‘t help. The code it self isn‘t that complex any more so i hoped that the problem would be obvious… just not for me ;)
I thought that i maybe do something wrong while goibg to sleep?!
2025-08-20 12:03 AM
> I thought that i maybe do something wrong while goibg to sleep?!
I think a problem during recovery from sleep is more likely.
Sleep modes have some side effects on peripherals, which need re-initialisation steps in some instances.
It seems you are using VS as IDE, I have no experience with debugging in this environment.
I would suggest to set a breakpoint at the wake-up, perhaps you would need to instruction/assembly mode debugging.
I very rarely work on application that employ sleep-mode, so I can't give much hints - except of a thorough read of the respective reference manual section.
2025-08-21 1:18 PM
Hi,
i noticed, that the 2MHz for the MSI clock is to high for the low power sleep mode. Unfortunately it doesn't work neither. But i did find a work around which surprisingly works with the 2MHz as well. I just inserted another asm ("nop") after waking up (immediately after __wfi). And it definitely works - the mcu goes to sleep - i checked the current consumption.
Greetings.