2015-07-30 10:24 AM
Hello,
I tried to use the Timer interrupt. In the examples of the STM Discovery they used the HAL_TIM_PeriodElapsedCallback handle function. But with this does'nt work (The don't used HAL_NVIC_EnableIRQ(TIM2_IRQn), why?). Then I enabled the IRQ with HAL_NVIC_EnableIRQ(TIM2_IRQn). Now it calls everytime the Default Handler even if I implented the TIM2_IRQHandler function. What is the error I make?
//TIM2: APB1
// Timer channel 2 as base timer
void
timer2Init()
{
/* Variables */
TIM_HandleTypeDef initTimBase;
/* enable Clocks */
__HAL_RCC_TIM2_CLK_ENABLE();
// every 1ms an overflow
initTimBase.Instance = TIM2;
initTimBase.Init.CounterMode = TIM_COUNTERMODE_UP;
initTimBase.Init.Period = 32;
initTimBase.Init.Prescaler = 1344;
initTimBase.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
initTimBase.Init.RepetitionCounter = 0;
//HAL_TIM_Base_Start(&initTimBase);
//__HAL_TIM_CLEAR_IT(&initTimBase, TIM_IT_UPDATE);
HAL_TIM_Base_Init(&initTimBase);
HAL_TIM_Base_Start_IT(&initTimBase);
HAL_NVIC_SetPriority(TIM2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM2_IRQn);
}
void
TIM2_IRQHandler(
void
)
{
int
i = 0;
i++;
//HAL_TIM_IRQHandler(&initTimBase);
}
2015-07-30 10:28 AM
What is the error I make?
Are you doing this in a .CPP file?What part specifically are you using?2015-07-30 11:58 AM
I use a normal .c file.
I have a stm32f411re nucleo board.2015-07-30 12:27 PM
This is my new Code, but it calls everytime the Default Handler and not my TIM2_IRQHandler.
TIM_HandleTypeDef initTimBase;
//TIM2: APB1
// Timer channel 2 as base timer
void
timer2Init()
{
/* Variables */
/* enable Clocks */
__HAL_RCC_TIM2_CLK_ENABLE();
// every 1ms an overflow
initTimBase.Instance = TIM2;
initTimBase.Init.CounterMode = TIM_COUNTERMODE_UP;
initTimBase.Init.Period = 32;
initTimBase.Init.Prescaler = 1344;
initTimBase.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
initTimBase.Init.RepetitionCounter = 0;
HAL_TIM_Base_Init(&initTimBase);
//MspInit haben keinen Rückgabewert
HAL_TIM_Base_Start_IT(&initTimBase);
HAL_NVIC_SetPriority(TIM2_IRQn, 4, 1);
HAL_NVIC_EnableIRQ(TIM2_IRQn);
}
void
TIM2_IRQHandler(
void
)
{
HAL_TIM_IRQHandler(&initTimBase);
}
// just defined interrupt function
/**
* @brief Period elapsed callback in non blockfaceing mode
* @param htim : TIM handle
* @retval None
*/
void
HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
static
uint32_t
time
= 0;
time
++;
// 1sek
if
(!(
time
% 1000))
{
if
(htim->Instance == TIM2)
{
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
}
}
}
2015-07-30 12:48 PM
Setup the NVIC *before* calling HAL_TIM_Base_Start_IT(), because it's going to fire immediately
2015-07-31 11:48 AM
I tried that too but no changes.
#include <stdio.h>
#include ''diag/Trace.h''
#include ''stm32f411xe.h''
#include ''stm32f4xx_hal.h''
void
timer2Init();
// ----- main() ---------------------------------------------------------------
// Sample pragmas to cope with warnings. Please note the related line at
// the end of this function, used to pop the compiler diagnostics status.
#pragma GCC diagnostic push
#pragma GCC diagnostic ignored ''-Wunused-parameter''
#pragma GCC diagnostic ignored ''-Wmissing-declarations''
#pragma GCC diagnostic ignored ''-Wreturn-type''
TIM_HandleTypeDef initTimBase;
int
main(
int
argc,
char
* argv[])
{
/* Variables */
uint32_t i;
HAL_Init();
gpioInit();
timer2Init();
// Button: PC13
// LED: PA5
// Infinite loop
while
(1)
{
for
(i = 0; i<500000; i++){}
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
}
}
//TIM2: APB1
// Timer channel 2 as base timer
void
timer2Init()
{
/* enable Clocks */
__HAL_RCC_TIM2_CLK_ENABLE();
// every 1ms an overflow
initTimBase.Instance = TIM2;
initTimBase.Init.CounterMode = TIM_COUNTERMODE_UP;
initTimBase.Init.Period = 32;
initTimBase.Init.Prescaler = 1344;
initTimBase.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
initTimBase.Init.RepetitionCounter = 0;
HAL_TIM_Base_Init(&initTimBase);
//MspInit haben keinen Rückgabewert
HAL_TIM_Base_Start_IT(&initTimBase);
HAL_NVIC_SetPriority(TIM2_IRQn, 4, 1);
HAL_NVIC_EnableIRQ(TIM2_IRQn);
}
void
TIM2_IRQHandler(
void
)
{
HAL_TIM_IRQHandler(&initTimBase);
}
// just defined interrupt function
/**
* @brief Period elapsed callback in non blockfaceing mode
* @param htim : TIM handle
* @retval None
*/
void
HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
static
uint32_t
time
= 0;
time
++;
// 1sek
if
(!(
time
% 1000))
{
if
(htim->Instance == TIM2)
{
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
}
}
}
#pragma GCC diagnostic pop
// ----------------------------------------------------------------------------
2015-07-31 12:02 PM
Pasted code doesn't appear to reflect that, or the cause of it being multiply defined all of a sudden.
Ok, so remove one of the definitions. The auto-generation probably built the one in the stm32f4xx_it.c, review it, decide if it's doing materially what you're current one is doing, or not, and delete one of them.2015-08-01 12:58 PM
In my project folder in eclipse does not exist a file named stm32f4xx_it.c.
2015-08-01 7:17 PM
The error you posted earlier
./src/stm32f4xx_it.o:/home/martin/workspace/STM32_New/Debug/../src/stm32f4xx_it.c:12: first defined here
Has the file in/home/martin/workspace/STM32_New/src/stm32f4xx_it.cThe HAL/Cube stuff is outside of what I'm dealing with, the linker should provide some insight via the .MAP file, and you can examine the vector table, and perhaps a listing or disassembly of the created code.2015-08-02 12:28 PM
I created this file to test if it works. But it didn't. In my project there is any stm324fxx_it.c file