HAL_SPI_TransmitReceive
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-02 4:54 PM
I'm having some peculiar behavior using the polling mode spin routines (F3), so I took a look at the HAL code. I'm sending 8 bit data using an array of 8-bit quantities. Inside the TransmitReceive routine I see this:
HAL_SPI_TransmitReceive
(
SPI_HandleTypeDef
*
hspi
,
uint8_t
*
pTxData
,
uint8_t
*
pRxData
,
uint16_t
Size
\
,
uint32_t
Timeout
)
/* Transmit and Receive data in 8 Bit mode */
else
{
while
((hspi->TxXferCount > 0) || (hspi->RxXferCount > 0))
{
/* check TXE flag */
if
((hspi->TxXferCount > 0) && ((hspi->Instance->SR & SPI_FLAG_TXE) == SPI_FLAG_TXE))
{
if
(hspi->TxXferCount > 1)
{
hspi->Instance->DR = *((
uint16_t
*)hspi->pTxBuffPtr);
hspi->pTxBuffPtr +=
sizeof
(uint16_t);
hspi->TxXferCount -= 2;
}
There's just so much wrong with this code. First there's the cast from uint8_t * to uint16_t *-- really ? All of a sudden you're introducing non-aligned accesses. Then there's the assumption that I want to send a multiple of 2 bytes -- NO NO NO.It appears I'll have to write my own transmission SPI routines since I can't trust these libraries.Geoffrey- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-03 6:49 AM
Hi brown.geoffrey.001,
This IP version is supporting the Data packing: as Data Register is 16bit (DR), IP is able to compute two data (2* 8bits) to packet a nex ata (16bit)
so in case of 8bits data, data are sent by packet of 16bits (2 datas)
“
I'm having some peculiar behavior using the polling mode spin routines (F3)��
--> Otherwise, Can you describe clearly (in details) the issue/behavior that you faced.
-Hannibal-
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-03 12:20 PM
Sure -- suppose I want/need to send a single byte -- i.e. to check response of device. The library code will always send two.
Suppose I need to send a buffer with 9 bytes -- the library code will always send 10. BTW, the last byte will always be whatever garbage happens to be in memory.I don't understand why anybody thinks there is a performance advantage here. The peak rate is 20Mbps (2.5 Mbyte/second) which is significantly longer than the code overhead. Also, as a very general rule -- programmers expect an interface that takes an array of bytes to work properly with any number of bytes. While the M4 cores support unaligned accesses, it's absolute folly to build a general library that depends upon this behavior.Geoffrey- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-01 1:44 AM
Hi. Does this help at all:
https://community.st.com/0D50X00009XkfrtSAB
Seems there is some contention on the HAL 8/16bit access, but I wrote my own driver after experiencing issues. Code snippet available at the link.