2018-09-24 1:36 PM
Hello,
I have a very simple code. A two byte array that I need to send over SPI.
uint8_t my_array[2];
my_array[0] = 0x10;
my_array[1] = 0x01;
HAL_SPI_Transmit(&hspi1, my_array, 2, SPI_TIME_OUT);
// or
HAL_SPI_Transmit(&hspi1, my_array, 1, SPI_TIME_OUT);
The HAL reference guide does not specify in what format is the "Size" expected? Is it in bytes? or in a 16-bit word?
2018-09-24 2:15 PM
Look at the library source code, it is provided.
Pretty sure it is a unit count. If you configured the SPI in 16-bit mode it will be words, and bytes in 8-bit mode.
2018-11-29 12:58 PM
Disclaimer: Not an expert.
tl;dr : 16-bit words
Looking at the source code in stm32f4xx_hal_spi.c, the argument in question (1 or 2) is received as parameter uint16_t Size.
HAL_StatusTypeDef HAL_SPI_Transmit(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size, uint32_t Timeout)
uint16_t Size is assigned to both hspi->TxXferSize and hspi->TxXferCount.
/* Set the transaction information */
hspi->State = HAL_SPI_STATE_BUSY_TX;
hspi->ErrorCode = HAL_SPI_ERROR_NONE;
hspi->pTxBuffPtr = (uint8_t *)pData;
hspi->TxXferSize = Size;
hspi->TxXferCount = Size;
The routine loops through hspi->TxXferCount and decrements down to zero. I believe the answer to your question is found herein. DR is loaded with a 16-bit word along with decrement of TxXferCount; the load and decrement are 1-to-1. If Size was 8-bit char, we might assume it would be 2-to-1. This suggests the argument Size is 16-bit words.
/* Transmit data in 16 Bit mode */
while (hspi->TxXferCount > 0U)
{
/* Wait until TXE flag is set to send data */
if(__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_TXE))
{
hspi->Instance->DR = *((uint16_t *)pData);
pData += sizeof(uint16_t);
hspi->TxXferCount--;
}
else
{
/* Timeout management */
if((Timeout == 0U) || ((Timeout != HAL_MAX_DELAY) && ((HAL_GetTick()-tickstart) >= Timeout)))
{
errorcode = HAL_TIMEOUT;
goto error;
}
}
}
2018-11-29 1:17 PM
uint16_t Size in this context means between 0 and 65535 units, and is unrelated to the width of the transfer over the bus.
SpiHandle.Init.DataSize = SPI_DATASIZE_8BIT; // << THIS IS CONTROLLING