2015-03-03 7:23 AM
Hal_sd_readblocks not working correctly
2015-03-03 9:14 AM
woops, no message:
Ok so there was another thread where clive1 already helped me work through a number of issues (as well as other posters on other threads, thanks to all of you!) but I still have one strange issue that is different enough for me to want to post another thread so that you all might get a chance to see it.Essentially, When I use HAL_SD_writeblocks(xxx) it works just fine (fatfs calls this function, I do not do it directly). It writes in blocks of 512, and (so far as I know) will write as many blocks as it needs (for my current tests im only doing 1024 bytes).The problem comes in when I call f_read which in turn calls HAL_SD_readblocks(xxx) which has 2 strange errors:1) It reads half the bytes I specify eg I say read 512 and it reads 2562) It will only read a maximum of 1 block (512 bytes)Does anyone have any idea what could be happening?I have pullups on the lines, 100 nF dc caps on each VCC.This is an stm32f4xxx processor using keil and the stm32cube f4 v. 1.4 generated code.