cancel
Showing results for 
Search instead for 
Did you mean: 

HAL SAI cannot run quick enough for basic audio sampling?

RBamf.1
Associate III

I am trying to take a microphone sample every 62.5 microseconds (16,000Hz) which is the standard rate for audio files.

The problem i have found is that HAL_SAI_Receive_DMA() returns HAL_BUSY for some samples. So we dont receive the required 16,000 samples in the 1 second, it only manages 14750.

The SAI component can reach rates of 192KHz so it makes no sense that it cannot handle 16KHz? So how do i fix the problem of receiving HAL_BUSY?

Thanks!

Here is an example sketch running on an STML452RE:

#include <SoftwareSerial.h>
#include <Arduino.h>
#include <HardwareTimer.h>
 
#include "stm32l4xx.h"
#include "stm32l4xx_hal.h"
#include "stm32l4xx_hal_def.h"
#include "stm32l4xx_hal_gpio.h"
#include "stm32l4xx_hal_sai.h"
#include "stm32l4xx_hal_exti.h"
#include "stm32l4xx_hal_cortex.h"
 
#include "Sysclock_Config.h"
 
 
 
GPIO_InitTypeDef gpioInit;
SAI_HandleTypeDef saiHandle;
RCC_PeriphCLKInitTypeDef periphInit;
DMA_HandleTypeDef hdmaInit;
 
uint8_t	SAIDataBuffer[8] = { 0 };
HardwareTimer hardwareTimer(TIM3);
 
void assert_failed(uint8_t* inFileName, uint32_t line)
{
	char* fileNameAsString = (char*)inFileName;
	Serial2.println(F("*** [HAL ASSERT FAILED] ***"));
	Serial2.printf("%s\r\n", (char*)inFileName);
	Serial2.printf("%i\r\n", line);
}
void _Error_Handler(const char* file, int line)
{
	Serial2.println(F("*** [ERROR HANDLED] ***"));
	Serial2.printf("%s\r\n", file);
	Serial2.printf("%i\r\n", line);
}
 
extern "C"
{
	void HAL_SAI_TxHalfCpltCallback(SAI_HandleTypeDef* hsai)
	{
	}
 
	void HAL_SAI_TxCpltCallback(SAI_HandleTypeDef* hsai)
	{
	}
 
	void HAL_SAI_RxHalfCpltCallback(SAI_HandleTypeDef* hsai)
	{
	}
 
	void HAL_SAI_RxCpltCallback(SAI_HandleTypeDef* hsai)
	{
	}
 
	void HAL_SAI_ErrorCallback(SAI_HandleTypeDef* hsai)
	{
	}
 
	__weak void SAI1_IRQHandler(void)
	{
		HAL_SAI_IRQHandler(&saiHandle);
	}
 
	__weak void DMA2_Channel1_IRQHandler(void)
	{
		/* USER CODE BEGIN DMA2_Channel1_IRQn 0 */
 
		/* USER CODE END DMA2_Channel1_IRQn 0 */
		HAL_DMA_IRQHandler(&hdmaInit);
		/* USER CODE BEGIN DMA2_Channel1_IRQn 1 */
 
		/* USER CODE END DMA2_Channel1_IRQn 1 */
	}
}
 
void samplerCallback();
 
 
// the setup function runs once when you press reset or power the board
void setup()
{
	delay(5000);
 
	Serial2.begin(115200);
	Serial2.println("Starting");
 
 
	__HAL_RCC_GPIOB_CLK_ENABLE();
	__HAL_RCC_DMA2_CLK_ENABLE();
	__HAL_RCC_SAI1_CLK_ENABLE();
 
	gpioInit.Pin = GPIO_PIN_15 | GPIO_PIN_10 | GPIO_PIN_12;
	gpioInit.Mode = GPIO_MODE_AF_PP;
	gpioInit.Pull = GPIO_NOPULL;
	gpioInit.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	gpioInit.Alternate = GPIO_AF13_SAI1;
	HAL_GPIO_Init(GPIOB, &gpioInit);
 
	pinMode(PB1, OUTPUT);
	digitalWrite(PB1, LOW);
 
	saiHandle.Instance = SAI1_Block_A; // audio block A.
	saiHandle.Init.Protocol = SAI_FREE_PROTOCOL;
	saiHandle.Init.FirstBit = SAI_FIRSTBIT_MSB;
	saiHandle.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_16K;
	saiHandle.Init.AudioMode = SAI_MODEMASTER_RX; // block a must provide clock signals and receive from the data line.
	saiHandle.Init.Synchro = SAI_ASYNCHRONOUS;	// we only want to use this one audio block.
	saiHandle.Init.SynchroExt = SAI_SYNCEXT_DISABLE; // disable sychronizing the 2 audio blocks.
	saiHandle.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE; // assume to power the data?
	saiHandle.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE; // any frame length allowed.
	saiHandle.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY;	// used for interrupts.
	saiHandle.Init.MonoStereoMode = SAI_STEREOMODE; // mono mode only available in transmission mode.
	saiHandle.Init.CompandingMode = SAI_NOCOMPANDING; // telecommunications specification (not needed)
	saiHandle.Init.TriState = SAI_OUTPUT_NOTRELEASED; // assume the SAI is ma
	saiHandle.FrameInit.FrameLength = 64; // 64 bit frame. (2 slots)
	saiHandle.FrameInit.ActiveFrameLength = 32; // Frame synchronization active level length. (half the frame length)
	saiHandle.FrameInit.FSDefinition = SAI_FS_CHANNEL_IDENTIFICATION;
	saiHandle.FrameInit.FSPolarity = SAI_FS_ACTIVE_LOW;
	saiHandle.FrameInit.FSOffset = SAI_FS_BEFOREFIRSTBIT;
	saiHandle.SlotInit.FirstBitOffset = 0; // no offset in receive mode -> FBOFF <= (SLOTSZ - DS)
	saiHandle.SlotInit.SlotSize = SAI_SLOTSIZE_32B; // 32 bits per slot to contain the 32 data bits (24 data, 8 zeroed)
	saiHandle.SlotInit.SlotNumber = 2;
	saiHandle.SlotInit.SlotActive = SAI_SLOTACTIVE_ALL;
 
	hdmaInit.Instance = DMA2_Channel1;
	hdmaInit.Init.Request = DMA_REQUEST_1;
	hdmaInit.Init.Direction = DMA_PERIPH_TO_MEMORY;
	hdmaInit.Init.PeriphInc = DMA_PINC_DISABLE;
	hdmaInit.Init.MemInc = DMA_MINC_ENABLE;
	hdmaInit.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
	hdmaInit.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
	hdmaInit.Init.Mode = DMA_NORMAL;
	hdmaInit.Init.Priority = DMA_PRIORITY_VERY_HIGH;
	if (HAL_DMA_Init(&hdmaInit) != HAL_OK)
	{
		Error_Handler();
	}
 
	/* Several peripheral DMA handle pointers point to the same DMA handle.
	 Be aware that there is only one channel to perform all the requested DMAs. */
	__HAL_LINKDMA(&saiHandle, hdmarx, hdmaInit);
	__HAL_LINKDMA(&saiHandle, hdmatx, hdmaInit);
 
	HAL_NVIC_SetPriority(DMA2_Channel1_IRQn, 0, 0);
	HAL_NVIC_EnableIRQ(DMA2_Channel1_IRQn);
 
	HAL_NVIC_SetPriority(SAI1_IRQn, 0, 0);
	HAL_NVIC_EnableIRQ(SAI1_IRQn);
 
 
	HAL_StatusTypeDef saiStatus = HAL_SAI_InitProtocol(&saiHandle,
													   SAI_I2S_STANDARD, // runs the SAI_InitI2S() function.
													   SAI_PROTOCOL_DATASIZE_24BIT,// 24 bits (24 bit is standard for I2S).
													   2);			 // number of slots per frame - 1
 
 
	__HAL_SAI_ENABLE(&saiHandle);
 
	if (saiStatus != HAL_OK)
	{
		Serial2.println("SAI ERROR");
		while (1) {}
	}
	else
	{
		Serial2.println("Sai init ok.");
	}
 
	hardwareTimer.setMode(1, TIMER_OUTPUT_COMPARE, NC); // remove this for new version of STM32Dino, required version 1.8.0.
	hardwareTimer.setOverflow(16000, HERTZ_FORMAT);
	hardwareTimer.detachInterrupt();
	hardwareTimer.attachInterrupt(samplerCallback);
	hardwareTimer.resume();
 
	Serial2.flush();
 
	start = millis();
}
 
 
 
int32_t GetSample()
{
	uint8_t a1 = SAIDataBuffer[0];
	uint8_t b1 = SAIDataBuffer[1];
	uint8_t c1 = SAIDataBuffer[2];
	uint8_t d1 = SAIDataBuffer[3];
 
	uint8_t a2 = SAIDataBuffer[4];
	uint8_t b2 = SAIDataBuffer[5];
	uint8_t c2 = SAIDataBuffer[6];
	uint8_t d2 = SAIDataBuffer[7];
 
	// value as signed 24 bit integer
	int32_t slot24sb = 0;
	slot24sb = slot24sb | (a1 << 8);
	slot24sb = slot24sb | (b1 << 16);
	slot24sb = slot24sb | (c1 << 24);
	slot24sb = slot24sb >> 8;
 
	return slot24sb;
}
 
int num_samples = 0;
 
void samplerCallback(void)
{
	HAL_StatusTypeDef rxResponse;
 
	rxResponse = HAL_SAI_Receive_DMA(&saiHandle, SAIDataBuffer, 2U);
 
	int sample = GetSample();
 
	if (rxResponse != HAL_OK)
	{
		//Serial2.println("Error in SAI");
	}
	else
	{
		num_samples++;
	}
}
 
 
// the loop function runs over and over again until power down or reset
void loop()
{
	if (millis() - start > 1000)
	{
		Serial2.println(num_samples);
		while (1) {}
	}
}

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
RBamf.1
Associate III

The issue was that the Master Clock Divider was not configured correctly and that samples need to be handled in the "Transfer Complete" callback. Thank you @Community member​ and @Community member​