2017-05-18 11:28 AM
I'm using
STM32Cube_FW_L4_V1.6.0 for long bulk transfers (up to 4096 bytes). When the stm32 receives a packet longer that 64 bytes, HAL_PCD_EP_GetRxCount returns a number 1-64 (e.g. a packet of 1024 returns a length of 64). The received data seem to be correct, so I'm confused about the incorrect packet length (plus it's impossible to detect errors !). Has anybody seen a similar problem ?
Geoffrey
2017-05-19 2:35 AM
Hi
Brown.Geoffrey
,Please use the last STM32CubeL4 firmware version 1.8.0 as contains update on HAL PCD driver.
Then, keep us updated about your progress on this.
Thanks
Imen
2017-05-19 5:32 AM
I've moved to the latest 1.8.0 firmware, without a change. Here's what I am attempting to accomplish. I have written a bulk driver and want to receive large packets. In my code I call prepare receive:
USBD_LL_PrepareReceive(pdev,
BULK_OUT_EP,
hcdc->RxBuffer,
hcdc->RxLength);�?�?�?�?�?�?�?�?
In the specific case that is causing me trouble, hcdc->RxLength is greater than 64 bytes (e.g. 1024). In my ***_DataOut function, I attempt to capture the length of data received.
hcdc->RxLength = USBD_LL_GetRxDataSize(pdev, epnum);�?�?�?
USBD_LL_GetRxDataSize is simply a wrapper for HAL_PCD_EP_GetRxCount.
***_DataOut is called by the usual chain
HAL_PCD_DataOutStageCallback -->
USBD_
LL_Da
taOutStage --> ***_DataOut
The problem is that USBD_LL_GetRxDataSize seems to return the size of literally the last packet (e.g. 64 bytes or less) received rather than the total amount received since the last call to USBD_LL_PrepareReceive.
Either I'm misunderstanding the intended behavior of USBD_LL_GetRxDataSize (not unlikely: as a side note, to the STM documentation team, procedure prototypes document syntax, but not semantics), or there is a but in the libraries. If the former, please give a hint about how to accomplish my goal. If the later, please give a workaround.
2017-05-19 5:55 AM
ok, I hate having to grovel around in the HAL code just to figure out what is going on. Here's a bit of stm32l4xx_hal_pcd.c that seems wrong (around line 1585):
/*multi-packet on the NON control OUT endpoint*/
ep->xfer_count+=count;
ep->xfer_buff+=count;
if ((ep->xfer_len == 0) || (count < ep->maxpacket))
{
/* RX COMPLETE */
HAL_PCD_DataOutStageCallback(hpcd, ep->num);
}
else
{
HAL_PCD_EP_Receive(hpcd, ep->num, ep->xfer_buff, ep->xfer_len);
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
It seems the intent is to repeatedly call HAL_PCD_EP_Receive until the full packet is received. The code moves the buffer pointer (line 3), but in line 12 continues to provide the original length. Looks like a potential buffer overrun
(hint: it should probably be ep->xfer_len - ep->xfer_count).
2017-05-19 8:24 AM
Ok, I see the driver bug now. In the call to HAL_PCD_EP_Receive above, ep->xfer_count is reset to zero:
HAL_StatusTypeDef HAL_PCD_EP_Receive(PCD_HandleTypeDef *hpcd, uint8_t ep_addr, uint8_t *pBuf, uint32_t len)
{
PCD_EPTypeDef *ep = NULL;
ep = &hpcd->OUT_ep[ep_addr & 0x7F];
/*setup and start the Xfer */
ep->xfer_buff = pBuf;
ep->xfer_len = len;
ep->xfer_count = 0;
ep->is_in = 0;
ep->num = ep_addr & 0x7F;
if ((ep_addr & 0x7F) == 0 )
{
USB_EP0StartXfer(hpcd->Instance, ep, hpcd->Init.dma_enable);
}
else
{
USB_EPStartXfer(hpcd->Instance, ep, hpcd->Init.dma_enable);
}
return HAL_OK;
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
So, it behaves exactly as I said -- only the length of the last received packet is preserved. All that business of incrementing ep->xfer_count is for naught. Here's a dirty fix:
/*multi-packet on the NON control OUT endpoint*/
ep->xfer_count+=count;
ep->xfer_buff+=count;
if ((ep->xfer_len == 0) || (count < ep->maxpacket))
{
/* RX COMPLETE */
HAL_PCD_DataOutStageCallback(hpcd, ep->num);
}
else
{
uint32_t tmp = ep->xfer_count;
HAL_PCD_EP_Receive(hpcd, ep->num, ep->xfer_buff, ep->xfer_len - tmp);
ep->xfer_count = tmp;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
I hope that ST will do the right thing and test their PCD code a bit more thoroughly.
BTW, the same bugs exist for HAL_PCD_EP_Transmit, and a similar fix is required if xfer_count is expected to be meaningful, and it to eliminate the possibility of a buffer overrun.
2017-05-19 11:30 AM
Thank you
Brown.Geoffrey
for your contribution.Your reported issue is underinvestigation and I will keep you informed about the taken actions/explanation if needed.
Thanks
Imen