cancel
Showing results for 
Search instead for 
Did you mean: 

HAL Full duplex USART kluge fix

David Pekin
Senior
Posted on February 18, 2018 at 06:18

It turns out that the Hal example  two boards com DMA works only in a simplex mode. The USART is put in DMA rx mode and then, after a packet is received, it reinitializes the USART handle, sends a response, reinitializes the USART handle again and then goes into DMA rx mode again.  This works fine for a command response protocol but I needed to be able to transmit packets asynchronously while supporting the cmd/rsp protocol.   Note that the Hal implementation CAN handle repeated DMA transmits in succession correctly.  (Obviously it should work full duplex but it doesn’t)

So, I could dive into fixing the Hal library but I decided a more pragmatic and faster approach to my solution (full duplex USART functionality) was to use 2 usarts to make a single full duplex channel.  Since I had a working cmd/rsp channel, I added a second USART that I would only send on (repeated DMA rx works fine). 

So, I disconnected the TX signal from Usart1 that handles the cmd/rsp protocol and I connected the TX signal from Usart2 to the driver chip.  So I send the Rsp packet the cmd/rsp channel (USART1) to both USART 1 and USART2.  The usart1 tx line is disconnected but we send it to keep the cmd/rsp channel working within the Hal limitations. We also send the rsp packet to USART 2 which is connected to the driver chip so it is transmitted. A sync packets also can be sent to usart2.  As I said, multiple DMA transmits work with the Hal libs so in this design, 

usart 1 handles incoming commands and usart 2 handles all outgoing responses and a sync packets.

This was a faster way to a full duplex solution versus debugging the Hal libs.

i hope this helps

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0