cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_ADC_PollForConversion gets stuck

dfshea
Associate III

I'm writing software that involves reading a single ADC value from my STM32H7R3V8H6, however it is getting stuck in HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);.

If i switch the delay to a smaller value it runs through but it still returns a timeout.

while (1)
  {
		HAL_ADC_Start(&hadc1);
		HAL_ADC_PollForConversion(&hadc1, 100);
		adc1Data = HAL_ADC_GetValue(&hadc1);
		HAL_ADC_Stop(&hadc1);
		//readT(&engine, 0);
		//readP(&engine, 0);
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
  }

static void MX_ADC1_Init(void)
{

  /* USER CODE BEGIN ADC1_Init 0 */

  /* USER CODE END ADC1_Init 0 */

  ADC_MultiModeTypeDef multimode = {0};
  ADC_ChannelConfTypeDef sConfig = {0};

  /* USER CODE BEGIN ADC1_Init 1 */

  /* USER CODE END ADC1_Init 1 */

  /** Common config
  */
  hadc1.Instance = ADC1;
  hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
  hadc1.Init.Resolution = ADC_RESOLUTION_12B;
  hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
  hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
  hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
  hadc1.Init.LowPowerAutoWait = DISABLE;
  hadc1.Init.ContinuousConvMode = DISABLE;
  hadc1.Init.NbrOfConversion = 1;
  hadc1.Init.DiscontinuousConvMode = DISABLE;
  hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
  hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
  hadc1.Init.SamplingMode = ADC_SAMPLING_MODE_NORMAL;
  hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
  hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
  hadc1.Init.OversamplingMode = DISABLE;
  if (HAL_ADC_Init(&hadc1) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure the ADC multi-mode
  */
  multimode.Mode = ADC_MODE_INDEPENDENT;
  if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Regular Channel
  */
  sConfig.Channel = ADC_CHANNEL_0;
  sConfig.Rank = ADC_REGULAR_RANK_1;
  sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
  sConfig.SingleDiff = ADC_SINGLE_ENDED;
  sConfig.OffsetNumber = ADC_OFFSET_NONE;
  sConfig.Offset = 0;
  sConfig.OffsetSign = ADC_OFFSET_SIGN_NEGATIVE;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN ADC1_Init 2 */

  /* USER CODE END ADC1_Init 2 */

}
17 REPLIES 17

I misspoke, it doesn't return a timeout, it simply stays there forever. I looked into the code and it gets stuck in the loop that I put previously. That loop looks like it will return HAL_ERROR after some time, but its a very large amount of time.

The ADC clock is enable from calling  MX_ADC1_Init>HAL_ADC_Init>HAL_ADC_MspInit

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Chris21
Senior III

Looks like the H7 is a bit different as far as the ADC Clock, it's set in RCC domain 3 kernel clock configuration register (RCC_D3CCIPR):

Chris21_0-1741127127185.png

 

Chris21_1-1741127166620.png

 


@dfshea wrote:

I misspoke, it doesn't return a timeout, it simply stays there forever. I looked into the code and it gets stuck in the loop that I put previously. That loop looks like it will return HAL_ERROR after some time, but its a very large amount of time.


Did you use 100ms for the timeout?

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

For the ADC calibration I didn't see any option for a timeout, just inputting the ADC handle and ADC_SINGLE_ENDED.

Hello @dfshea 

Could you please share your project so that we can assist you more effectively?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

@dfshea wrote:

For the ADC calibration I didn't see any option for a timeout, just inputting the ADC handle and ADC_SINGLE_ENDED.


No, i'm at talking about when you call HAL_ADC_PollForConversion

If you pass 100ms and it doesn't timeout, then you have two issues. 

1. the ADC_FLAG_EOC flag isn't being set so you're stuck in the while loop.

2. HAL Tick isn't incrementing so it doesn't timeout.

Sounds like maybe something wasn't set up correctly or modified from default. Upload your IOC file

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

I see, yes, when I call HAL_ADC_PollForConversion it does indeed time out after 100ms. I've attached the IOC below, let me know if you need anything else.