cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO Port configuration register - max speed

alanrouse9
Associate II
Posted on December 01, 2010 at 14:27

GPIO Port configuration register - max speed

4 REPLIES 4
Posted on May 17, 2011 at 14:16

Slew Rate control, slower rates will also reduce the overshoot and ringing, as the pins are driven less aggressively.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
John F.
Senior
Posted on May 17, 2011 at 14:16

Lower electrical noise because of reduced slew rate helps analogue and also improves chances of passing EMC (radiated noise) tests.

Andrew Neil
Evangelist III
Posted on May 17, 2011 at 14:16

''improves chances of passing EMC (radiated noise) tests.''

Also conducted noise?
dthedens2
Associate II
Posted on May 17, 2011 at 14:16

And higher frequency setting can cause higher current draw