2012-10-29 12:54 AM
I have a problem. I set my GPIO port pins on GPIOA. When I wanted to lock them I used GPIO_PinLockConfig function, but when the function passed through. It has done nothing. My pins in LCKR lock register was not locked? Why? I had set AHBPeriph clock because before I set GPIOA TypeDef register and it worked.
Thanks. Martin.2012-10-29 06:59 AM
This worked for me in Keil, returns 0x00010004, STM32F0-Discovery board
uint32_t testlock(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable the GPIO Clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* Configure the GPIO pin */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Lock the GPIO pin */
GPIO_PinLockConfig(GPIOA, GPIO_Pin_2);
return(GPIOA->LCKR);
}
2012-10-29 07:32 AM
Thanks for your reply
Sequence of the code I wrote is the same as you wrote here. 1. I tried to debug it by hardware degugger ST LINK and I watched LCKR register of given PORT in system viewer windows. But nothing changed in LCKR register and as I mentioned I used the same sequence as you in your example. 2. When I tried to debug it by software KEIL simulator it everything worked well. All locked bits were set in and LCKK bit was set. I watched it in system viewer windows again. I am little bit afraid, that my MCU is little bit destroyd. At least LCKR register. I see it, that I will have to try it again. Even though thanks for your help.2012-10-31 03:46 AM
That one below does not work for me. Clive1 would you be able to help me?
This worked for me in Keil, returns 0x00010004, STM32F0-Discovery board
uint32_t testlock(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable the GPIO Clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* Configure the GPIO pin */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Lock the GPIO pin */
GPIO_PinLockConfig(GPIOA, GPIO_Pin_2);
return(GPIOA->LCKR);
}
2012-10-31 03:50 AM
Sorry it did not add printscreens. Why?