2016-05-08 9:15 PM
How can we get the timestamp information in a better way in ms - using systick configured @1ms and calling HAL_GetTick() to get the time in ms or using RTC?
#systick #priority #!stm32f4-!stm32f401-!rtc #stm32f42016-05-08 10:25 PM
time_t getRTCAsUnixTime(void) {
RTC_DateTypeDef date;
RTC_TimeTypeDef time;
HAL_RTC_GetTime(&hrtc, &time, FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &date, FORMAT_BIN);
struct tm tm = {
tm_sec: time.Seconds,
tm_min: time.Minutes,
tm_hour: time.Hours,
tm_mday: date.Date,
tm_mon: date.Month - 1,
tm_year: date.Year + 100,
tm_isdst: 0
};
return mktime(&tm);
}
volatile uint64_t utc; // mS since epoch
void HAL_SYSTICK_Callback(void) {
// other stuff here that has to be done each ms
++utc;
}
utc = (uint64_t)getRTCAsUnixTime() * 1000;
2016-05-09 1:36 AM
Hi,
struct tm tm = {
tm_sec: time.Seconds,
tm_min: time.Minutes,
tm_hour: time.Hours,
tm_mday: date.Date,
tm_mon: date.Month - 1,
tm_year: date.Year + 100,
tm_isdst: 0
is
struct tm tm correct?
code is not compilable.2016-05-09 2:11 AM
''How can we get the timestamp information in a better way''
''Better'' than what?In what way(s), exactly, do you want it to be ''better''? Or, in other words, how do you think your current way is inadequate?2016-05-09 3:29 AM
2016-05-09 5:56 AM
As explained here several times the issue with SysTick is that it must PREEMPT, which is not the same as the classic ''priority'' mindset. You need to adjust the Priority Grouping, and reconfigure the handler settings, so the interrupt occurs even if you are in other interrupts spinning.
Better yet, don't use a software timer for these purposes, and don't idle in interrupts. Consider using a 32-bit timer (TIM2) clocking at 1 MHz (1 us) or a fractional second as accommodated by the 16-bit prescaler. If the chip powers down in STANDBY you'd need to use the RTC, but where it is just the CPU sleeping and the TIM keeps clocking, a timer would be fine. Perhaps the code example doesn't compile because it uses C++ like syntax rather than strict C. Check your compiler option settings, or just add some bracketed scope.2016-05-09 7:44 AM
2016-05-12 12:19 AM
= 49 days.?
what will be the value after 49 days? 0? can HAL_GetTick() return Zero in between in any case without shutting down the system?2016-05-12 12:53 AM
It will roll over, and provided you do the 32 bit unsigned math properly this will all work fine unless your desired timeout actually exceeds 50 days.
With two time stamp values a and b, delta = b - a, delta will be the elapsed ticks. Do, and understand, the math.2016-05-12 1:07 AM
yes I am taking the elapsed ms(ticks) as delta
if((HAL_GetTick() - oldTimeTick) >= 1000) {//do task}oldTimeTick is of uint32 types. , Here as you said there will not be any reset or rollover condition before ~49 days.Right?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.