2018-10-26 12:47 AM
Hello,
My aim is to get data from two ADC channels in order to extrat data into a file. I want then to analyze data with Matlab.
For now I achieve to see the two signals in my debugger but I can't manage to extract them from there.
I am using a Nucleo F411RE demoboard with TrueStudio. The initial code have been generated with CubeMX.
The signals are squared with a 37kHz frequency, so that I want to acquire with a minimum sampling frequency of 300kHz.
I wanted to use fopen, write, fclose to put data into a file but it seems not to work. I don't know why, I can't find the file if it is created or not.
Here is my main.c code
******************************************************************************
//* @file : main.c
//* @brief : Main program body
******************************************************************************
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32f4xx_hal.h"
#include "adc.h"
#include "dma.h"
#include "usart.h"
#include "gpio.h"
/* Private variables ---------------------------------------------------------*/
uint8_t channel=1;
uint32_t adc[2], buffer[2];
uint16_t tab1[20000];
uint16_t tab2[20000];
uint32_t n1=0;
uint32_t n2=0;
float vsense=3300/4095;
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
adc[channel]=buffer[0];
if (channel == (2-1) ){
tab2[n2]=adc[channel];
n2++;
channel = 0;
}
else{
tab1[n1]=adc[channel];
n1++;
channel++;
}
}
int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_USART1_UART_Init();
HAL_ADC_Start_DMA(&hadc1, buffer, 1);
HAL_ADC_Start_IT(&hadc1);
/*
FILE *pFile;
pFile= fopen("test.txt", "w");
fprintf(pFile, "Hello file");
if (pFile != NULL)
{
fclose(pFile);
}
else
{
printf("Could not open the file. \n");
}
*/
while (1)
{
HAL_ADC_Start_IT(&hadc1);
HAL_Delay(1);
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
/**Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 200;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
/**
* @brief This function is executed in case of error occurrence.
* @param file: The file name as string.
* @param line: The line in file as a number.
* @retval None
*/
void _Error_Handler(char *file, int line)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
while(1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
2018-10-28 01:44 PM
Choose only 1 from
2018-10-29 01:08 AM
Yes, it's working.
Actually I put the data into two tabs tab1 and tab2. I want to extract them to a file .txt or .bin but the functions fopen, fclose don't semm to work with TrueSudio.
Another thing, I would like to know the speed of putting data into tabs. I know that my acquisition speed from the ADC is about 1,6 Msps but after this I don't know anything.
Thanks,
Philippe