2014-01-06 12:20 PM
Hello Everyone,
I have been having this issue for a while on a STM32L100-Discovery board, apparently on reset there is always a garbage character transmitted to the terminal. After the reset the USART works fine. My code to initialize the USART is below, any help or ideas would be welcome and appreciated. Thanks in advance.GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; int c = 0x1FFFF; /** * USART1 GPIO Configuration PA9 ------> USART1_TX PA10 ------> USART1_RX */ /*Enable or disable the AHB1 peripheral clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); /*Configure GPIO pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9|GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); /*Configure GPIO pin alternate function */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1); /*Configure GPIO pin alternate function */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1); USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; /* USART configuration */ USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1, DISABLE); NVIC_PriorityGroupConfig( NVIC_PriorityGroup_4 ); /* Enable USART Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 8; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 8; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable USART */ USART_Cmd(USART1, ENABLE); // enable interrupt for uart USART_ITConfig(USART1, USART_IT_TXE, DISABLE); USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);On first printf we see, second printf is fine:ÿBeginSuccess2014-01-06 1:00 PM
Would an external pull-up on the TX line help? Or some reordering of the pin configuration and enablement?
Your goal is to avoid seeing a phantom start bit, observe condition with scope to better understand the glitch behaviour.2014-01-07 5:56 AM
Thanks Clive I will take a look at it today on the scope and see what is going on and definitely try the pull-up resistor.
Thanks Again.George2014-01-07 6:08 AM
Thanks Clive again, a 10k pull-up on the transmit line got rid of the phantom data on reset.