Function for printing values
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-23 8:54 AM
Hello,
I'm working with the NUCLEO-F722ZE EVB on STM32CubeIDE.
I want to use the main USB connection to the PC as a UART.
The default CubeMX pin configuration already has PD8 and PD9 configured as a UART, so I proceeded with code generation (the auto generated main.c file is attached).
What's the recommended function I to print characters to the PC terminal over the UART ?
For example, if I want to send: "Hello World".
What would be the code for it ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-23 9:27 AM
You can plumb it so printf()/puts() works, and it would pull in extra library code.
You can write your own StringOut() type function to interact with the USART registers,
or use HAL functions
void StringOut(char *s)
{
HAL_UART_Transmit(&huart3, (void *)s, strlen(s), 1000);
}
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-23 11:50 AM
Thanks,
This is what I used:
char buffer[] = "Hello World";
HAL_UART_Transmit(&huart3, buffer, sizeof(buffer), 0xFFFF);
I turned on "Putty" configured it to 115200 (the same way as the CubeMx is).
Instead of seeing "Hello World" printed on the screen I see garbage (attached).
Generally I'd guess it's a baud rate mismatch - but as I said the setting in the CubeMx matches the Putty.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-24 10:39 AM
@Community member​ ,
Can you please show an example of what you mean by:
"plumb it so printf()/puts() works, and it would pull in extra library code."
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-24 11:34 AM
Understand that forums are a land of repetitive questions, a search might yield the specific implementation details for the tools you have chosen to use.
UART_HandleTypeDef UartHandle = {0};
//****************************************************************************
// Hosting of stdio functionality through USART (Keil)
//****************************************************************************
/* Implementation of putchar (also used by printf function to output data) */
int SendChar(int ch) /* Write character to Serial Port */
{
HAL_UART_Transmit(&UartHandle, (void *)&ch, 1, 1000);
return(ch);
}
//****************************************************************************
#include <rt_misc.h>
int fputc(int ch, FILE *f) { return (SendChar(ch)); }
int ferror(FILE *f)
{
/* Your implementation of ferror */
return EOF;
}
void _ttywrch(int ch) { SendChar(ch); }
void _sys_exit(int return_code)
{
label: goto label; /* endless loop */
}
//****************************************************************************
void USART2_Init(uint32_t BaudRate) // USART2 TX1/RX1
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
__USART2_CLK_ENABLE();
__GPIOA_CLK_ENABLE();
/* UART RX/TX GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_9 | GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_USART2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*## Configure the UART peripheral ######################################*/
/* Put the USART peripheral in the Asynchronous mode (UART Mode) */
/* UART configured as follow:
- Word Length = 8 Bits
- Stop Bit = One Stop bit
- Parity = NO parity
- BaudRate = 115200 baud
- Hardware flow control disabled (RTS and CTS signals) */
UartHandle.Instance = USART2;
UartHandle.Init.BaudRate = BaudRate;
UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
UartHandle.Init.Mode = UART_MODE_TX_RX;
UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
#ifdef UART_ONE_BIT_SAMPLE_DISABLE
UartHandle.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
#endif
if (HAL_UART_Init(&UartHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
}
//****************************************************************************
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-24 12:50 PM
if you use the usb to usart service from stlink, tune on pc side the baudrate which will control stlink uart. your target should match. for debug, i build my own printf.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-24 1:36 PM
It is tuned...
The baudrate on my PC is the same as the configuration at the MXCube.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-24 4:28 PM
@clive1 (NFA Crew) (Community Member)​ ,
When defining the function you suggested - I get the following warning :
"implicit declaration of function strlen"
It points to this line:
HAL_UART_Transmit(&huart3, (void *)s, strlen(s), 1000);
Should I declare the header file that defines "strlen" ?
Can I use "sizeof" instead ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-24 11:09 PM
Personnaly, LL is more practical for USART than HAL especially for single byte chunks
Do send your output message every 1 second to monitor the output.
If you have a scope, check the duration of the start bit and compare it with the baud rate.
I don't know putty and if it uses unicode or ASCII, can you try with Teraterm?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-24 11:10 PM
if the baudrate is wrong at least should your get something else than the same char repeteadly... and it's even not a wrong ASCII code...