cancel
Showing results for 
Search instead for 
Did you mean: 

FSMC NAND flash speed?

childresss
Associate II
Posted on April 07, 2015 at 19:24

What transfer rate (read and write) can be expected for an FSMC interface to NAND flash, 8 bit data path, DMA, STM32F4xx at either 48 or 168MHz? Is it heavily influenced by choice of NAND flash chip vendor/part?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on April 07, 2015 at 22:22

The FSMC is merely a conduit to the data buffers on the device, the speed at which it can fetch blocks, erase and write them will depend on the Flash architecture and geometry. The higher density memory is inherently less reliable and has more complicated/robust error correction schemes. The newer devices having built-in ECC syndrome generation/checking hardware, with correction performed by software on the host. Probably won't need the STM32's ECC generation/checking.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..