2013-04-16 11:26 PM
Hi all,
I have a ST7753S 8 bit bus, 8080 style, hooked up to STM32F103VE FSMC with config as below. However I find that there are 2 bytes being written every time I write a char. Is this how it works, or am I doing sometimne wrong? Thanks for any assistance. Cheers. Pete L. static void LCD_FSMCConfig(void) { FSMC_NORSRAMInitTypeDef FSMC_NORSRAMInitStructure; FSMC_NORSRAMTimingInitTypeDef FSMC_NORSRAMTimingInitStructure; /* FSMC init*/ FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM1; FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable; FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_SRAM; FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_8b; FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low; FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState; FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;static void LCD_FSMCConfig(void)
{
FSMC_NORSRAMInitTypeDef FSMC_NORSRAMInitStructure;
FSMC_NORSRAMTimingInitTypeDef FSMC_NORSRAMTimingInitStructure;
/* FSMC init*/
FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM1;
FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable;
FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_SRAM;
FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_8b;
FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;
FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState;
FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable;
FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable;
FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable;
/* FSMC ReadWrite Timing */
FSMC_NORSRAMTimingInitStructure.FSMC_AddressSetupTime = 15;
FSMC_NORSRAMTimingInitStructure.FSMC_AddressHoldTime = 15;
FSMC_NORSRAMTimingInitStructure.FSMC_DataSetupTime = 15;
FSMC_NORSRAMTimingInitStructure.FSMC_BusTurnAroundDuration = 15;
FSMC_NORSRAMTimingInitStructure.FSMC_CLKDivision = 0x00;
FSMC_NORSRAMTimingInitStructure.FSMC_DataLatency = 0x00;
FSMC_NORSRAMTimingInitStructure.FSMC_AccessMode = FSMC_AccessMode_A;
FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &FSMC_NORSRAMTimingInitStructure;
/* FSMC Write Timing */
FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &FSMC_NORSRAMTimingInitStructure;
FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure);
/* Enable FSMC Bank4_SRAM Bank */
FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM1, ENABLE);
} FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable;
FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable;
FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable;
/* FSMC ReadWrite Timing */
FSMC_NORSRAMTimingInitStructure.FSMC_AddressSetupTime = 15;
FSMC_NORSRAMTimingInitStructure.FSMC_AddressHoldTime = 15; FSMC_NORSRAMTimingInitStructure.FSMC_DataSetupTime = 15;
FSMC_NORSRAMTimingInitStructure.FSMC_BusTurnAroundDuration = 15;
FSMC_NORSRAMTimingInitStructure.FSMC_CLKDivision = 0x00;
FSMC_NORSRAMTimingInitStructure.FSMC_DataLatency = 0x00;
FSMC_NORSRAMTimingInitStructure.FSMC_AccessMode = FSMC_AccessMode_A;
FSMC_NORSRAMTimingInitStructure.FSMC_AccessMode = FSMC_AccessMode_A;
FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &FSMC_NORSRAMTimingInitStructure;
/* FSMC Write Timing */
FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &FSMC_NORSRAMTimingInitStructure;
FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure);
/* Enable FSMC Bank4_SRAM Bank */
FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM1, ENABLE);
}
#fcsm-lcd
2013-04-17 12:57 AM
Sorry for the noise. Found the problem.
Was using //#define LCD_REG (*((volatile unsigned short *) 0x60000000)) /* RS = 0 */ //#define LCD_RAM (*((volatile unsigned short *) 0x60010000)) /* RS = 1 */ Changed to #define LCD_REG (*((volatile unsigned char *) 0x60000000)) /* RS = 0 */ #define LCD_RAM (*((volatile unsigned char *) 0x60010000)) /* RS = 1 */ So now, for example LCD_REG = ST7735S_SWRESET; sends only one byte. Cheers. Pete L.2013-11-24 12:35 PM
Pete L., Thank You!!!
The same problem, and this code helped me