cancel
Showing results for 
Search instead for 
Did you mean: 

FSMC DMA performance

martinpec19
Associate II
Posted on April 14, 2009 at 12:31

FSMC DMA performance

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
martinpec19
Associate II
Posted on May 17, 2011 at 13:09

Hello.

We are trying to connect CCD chip on STM32F103ZE.

The CCD is connected on port A(16 bit). We are generating DMA request with Timer T1 (capture event) with Pixel clock of CCD.

DMA is copying value from port A to FSMC connected external RAM (16 bit).

Our maximum troughtput is 3M transfers per second(to external RAM) and 6M transfers to internal ram. Processor is running on 72MHz with HCLK 72MHz also.

Is this maximum troughtput we can achive or we are missing something ?

Regards, Martin.