cancel
Showing results for 
Search instead for 
Did you mean: 

FSMC and SRAM Example halts

kisnemeth
Associate II
Posted on April 23, 2010 at 10:12

FSMC and SRAM Example halts

2 REPLIES 2
Nickname12657_O
Associate III
Posted on May 17, 2011 at 13:48

Hi,

You can refer to our latest Firmware published on web, we already include template files for Ride and run it on your board. I suspect that FSMC area is not configured or initialized in the right way.

Cheers,

STOne-32.

kisnemeth
Associate II
Posted on May 17, 2011 at 13:48

Hi STOne-32,

The latest v3.3.0 of firmware solved this problem. I used the old version becouse I'd had to implement a new function into an old project which used the v2.x.x firmware. Now I have to update the full project to v3.x.x. But at least it works!

Thank You,

Robert