cancel
Showing results for 
Search instead for 
Did you mean: 

FSMC and DMA causing dma error

giles
Associate II
Posted on December 09, 2008 at 11:34

FSMC and DMA causing dma error

This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
16-32micros
Associate III
Posted on May 17, 2011 at 12:51

Hi Tibo, Giles,

I will follow this interesting case about DMA and FSMC with my design mates

and let you posted on the progress once we get the required data for you.

Cheers,

STOne-32.

16-32micros
Associate III
Posted on May 17, 2011 at 12:51

Dear giles, tibo, all,

The limitation is confirmed in our silicon, This update is already requested and will be available in our (High density) errata in the coming days.

Description of the limitation :

--------------

Multi-master access are not supported on the FSMC memory

map (address space from 0x60000000-0xA0000FFF), Multi-master means: Dma1

/ Dma2 or Dma1 / CPU or Dma2 / CPU.

When multi-access are performed on this address space a dummy error

could be generated on the bus leading to either a CPU fail (Bus-fault

interrupt) or a DMA fail (error, transfer is stopped).

Workaround :

------------

If several masters (CPU, DMA1, DMA2) need to access the FSMC, the user

must ensure that the accesses are not concurrent by software and should

be sequential.

Cheers,

STOne-32.

[ This message was edited by: STOne-32 on 24-12-2008 14:00 ]

tibo
Associate II
Posted on May 17, 2011 at 12:51

hi ST1,

here is an open question from

http://www.st.com/mcu/forums-cat-7268-23.html

:

The FSMC interface has a 16 * 32 bit write buffer. How can this

buffer flushed by / sync with the program (by DMB/DSB??)? Or

is it possible to disable the buffer?

Perhaps it has something to do with the dma problem and you can discuss

(and answer) this with your engineers too.

tibo
Associate II
Posted on May 17, 2011 at 12:51

Hi St1,

there is still one essential question open: how is it possible to flush / sync the FSMC

buffer (16 word) with the program? Can I use DMB/DSB for this? Or is there a different

way to be sure, that all written data by the program is really written out of the buffer?

In our application we have a FPGA with dual ported SRAM connected to the FSMC.