cancel
Showing results for 
Search instead for 
Did you mean: 

FSMC acces mode

epassoni950
Associate II
Posted on September 22, 2010 at 17:24

FSMC acces mode

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
epassoni950
Associate II
Posted on May 17, 2011 at 14:08

Hello,

Is there somebody to help me to understand FSMC configuration.

Thank you in advance.

Eric
kashif
Associate II
Posted on May 17, 2011 at 14:08

yes there is a lot of timing difference between these two types of memory.

read this Application Note for complete understanding (AN2784)

http://www.st.com/stonline/products/literature/anp/14779.pdf

hope this will help. 

epassoni950
Associate II
Posted on May 17, 2011 at 14:08

Hello,

Thank you for your response.

Yes, I see AN2784 application note.

But for read timing, I can't see any difference between Figure 3 for Flash and Figure 6 for SRAM except for NADV signal which is don't care for non-multiplexed access.

For write timing, I can't see any difference between Figure 4 for Flash and Figure 6 for SRAM.

So I don't know the effect of choosing 10b (Flash) or 00b (Ram) for MTYP.

When I display signal on a oscilloscope, it seems there is no change when I use 10b or 00b for MTYP.

Eric