2013-06-06 06:59 AM
frequency capture
im trying to capture frequency from 0 to 100khz optical encoder . and here is my code doesn't seem to work. any help please im new to micro controller. im using stm32f100rb
&sharpinclude ''stm32f10x.h'' &sharpinclude ''stm32f10x_tim.h'' &sharpinclude ''stm32f10x_rcc.h'' &sharpinclude ''stm32f10x_gpio.h'' &sharpinclude ''misc.h'' unsigned int IC2Value, DutyCycle ,Frequency ; void RCC_Configuration(void) { RCC_APB1PeriphClockCmd (RCC_APB1Periph_TIM3, ENABLE); // clock configuration //RCC_APB2PeriphClockCmd (RCC_APB2Periph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC | RCC_APB2Periph_AFIO, ENABLE); } void GPIO_Configuration(void) { // GPIO configuration GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinRemapConfig( GPIO_FullRemap_TIM3, ENABLE ); // Map TIM3 to GPIOC } void NVIC_Configuration(void) { // NVIC configuration NVIC_InitTypeDef NVIC_InitStructure; NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init (& NVIC_InitStructure); } void TIM3_Configuration(void) { // TIMER configuration //TTIM_ICInitStructure (& TIM_ICInitStructure); TIM_ICInitTypeDef TIM_ICInitStructure; TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; // channel selection TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; // rising edge of the trigger TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; // correspondence between the pin and register TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; // input prescaler. Control in the number of input cycle time capture, if //TIM_ICInit(TIM3 , &TIM_ICInitStructure); /* Input signal frequency has not changed, will not change the measured period. Such as divided by 4, * each of the four input period before doing a capture, *so that the input signal does not change frequently, *Can reduce the frequency and software are constantly interrupted. */ TIM_ICInitStructure.TIM_ICFilter = 0x0; // filter settings, go through several cycles transition finds the stable waveform 0x0 to 0xF TIM_PWMIConfig (TIM3, & TIM_ICInitStructure); // the parameter configuration TIM peripheral information TIM_SelectInputTrigger (TIM3, TIM_TS_TI2FP2); // select IC2 always trigger source TIM_SelectSlaveMode (TIM3, TIM_SlaveMode_Reset) ;// TIM mode: update event triggers the rising edge of the signal to re-initialize the counter and trigger register TIM_SelectMasterSlaveMode (TIM3, TIM_MasterSlaveMode_Enable); // start the timer passive trigger TIM_Cmd (TIM3, ENABLE); // start TIM3 TIM_ITConfig (TIM3, TIM_IT_CC2, ENABLE); // Open interrupt } int main(void) { RCC_Configuration(); GPIO_Configuration(); TIM3_Configuration(); NVIC_Configuration(); void TIM3_IRQHandler (void) { IC2Value = TIM_GetCapture2 (TIM3); // read IC2 capture register, the count value is the PWM cycle if (IC2Value != 0) { DutyCycle = (TIM_GetCapture1 (TIM3) * 100) / IC2Value; // read IC1 to capture the value of the register, and calculate the duty cycle Frequency = 24000000 / IC2Value; // calculate the PWM frequency. } else { DutyCycle = 0; Frequency = 0; } TIM_ClearITPendingBit (TIM3, TIM_IT_CC2); // clear interrupt pending bit TIM } while(1) {} }2013-06-06 11:31 AM
what im trying to do is count the rpm (Speed) of the motor to give out pwm to control the motor. working on this for a month and half without any thing .. if any have a code or can do sthing hlp plz
2013-06-06 01:18 PM
Yeah, 45 days does seem a tad excessive, I'd probably use Input Capture mode and do a delta measurement between two edges against a fast time base. This would allow you to measure the period of one cycle, and thus the instantaneous frequency. 200 KHz a bit on the high side, for interrupting a CPU running at 24 MHz.
You'd probably also want a 32-bit timer, depends on how close to DC you want to measure, or how large a prescaler you can tolerate on a 16-bit counter. The F100 might be a problem in this regard. The other alternative is to count external pulses, and integrate over time, or gate/sample with a secondary timer. Would need to check quicker than 333ms to stay withing 16-bit and have 200KHz to DC range.2013-06-06 02:09 PM
hi clive1
thanx for replaying i really dont understand alot of things take easy with me plz 🙂 i have been reading alot specially in this side i almost red all your posts . delta measurement ?? but how can i implement this things how do i do it this my problem and can;t find any one to help me. i have another code for you for encoder interface (can i use this code to measure period or frequency?? here is the code// STM32 TIM3 Encoder Decoder (PC.06:A PC.07:B) VLDiscovery - sourcer32@gmail.com
#include ''stm32F10x.h''
#include ''STM32vldiscovery.h''
volatile int32_t Capture;
/**************************************************************************************/
void RCC_Configuration(void)
{
// clock for GPIO and AFIO (for ReMap)
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC | RCC_APB2Periph_AFIO, ENABLE);
// clock for TIM3
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
// PC.06 TIM3_CH1, PC.07 TIM3_CH2
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_PinRemapConfig( GPIO_FullRemap_TIM3, ENABLE ); // Map TIM3 to GPIOC
}
/**************************************************************************************/
void TIM3_Configuration(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_Period = 65535; // Maximal
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
// TIM_EncoderMode_TI1: Counter counts on TI1FP1 edge depending on TI2FP2 level.
TIM_EncoderInterfaceConfig(TIM3, TIM_EncoderMode_TI1, TIM_ICPolarity_Rising, TIM_ICPolarity_Rising);
TIM_Cmd(TIM3, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
TIM3_Configuration();
// TIM3->CNT contains current position
capture = TIM_GetCounter (TIM3) ;
while(1); // Do not exit
}
2013-06-06 04:20 PM
A delta measurement, ie a difference
So if you have an encoder setup up you could sample the value periodically, say every 1 ms, if the shaft is generating a 200 KHz signal this would appear as a delta measurement of 200 ticks up or down of the counter since the last measurement, 2000 for a 10 ms sampling. You could store that measurement in an array, and average 100 or 1000 samples. You should perhaps be seeking help from your colleagues, teachers, or whatever.2013-06-06 05:07 PM
i did he always buzy. this my final project have no collegee. can you show the part for measuring ?
2013-06-07 08:14 AM
You'll want to look at the SysTick examples in the firmware library.
Set up a 1 ms SysTick, and then in the SysTick_Handler() read the TIM3->CNT and compare the current value with the prior value.