2012-10-17 2:48 AM
Hi everyone!
I'm new to the world of microcontrollers,
these days I'm
doing my
first
espeienze
with
STM324
discovery,I'm reading
the various manuals
and trying out the
various
examples, but
I can not understand
how you set the
various frequencies
HSE
, HSIand
especially
APB1e
AP2
could you give me
directions?
thanks
2012-10-17 4:46 AM
You might want to review the clock tree in the manual.
HSI is fixed by the internal oscillator HSE is fixed by the external crystal APB1, and ABP2 are set to fractional (/1, /2, etc) of the AHB clock The PLL clock can get you any clock up to 168 MHz (VCO actually is twice that), which you can factor from the PLL settings with a 1-2MHz comparison frequency. You will typically set these parameters in system_stm32f4xx.c, and by the C initialization call SystemInit()2012-10-18 4:44 AM
thank you very much
!
between all the manuals I have a bit of confusion ...do you want tell me in which manual is the clock tree?2012-10-18 5:10 AM
The Reference Manual, Figure 9, Page 85